Difference between yocto setup distro version 1.6 and 1.7 .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between yocto setup distro version 1.6 and 1.7 .

1,815件の閲覧回数
veeranjaneyulug
Contributor III

Hi

I have one doubt i used yocto versions 1.6 and yocto version 1.7 for two projects.But main thing is we  used kernel 3.0.35/3.10.17 versions for yocto 1.6 used .linux kernel version 3.14.28 for yocto 1.7 used.

May i know what is the main difference between 1.6 and 1.7 .is it depends on linux kernel version?

Thanks & Regards

veeranjaneyulu

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,700件の閲覧回数
marcocavallini
Contributor V

Hi veeranjaneyulu,

generally speaking you should be able to replace the kernel version without problems keeping the same image created with older Yocto Project version. Consider that the YP version changes usually involve the GPU and/or graphical section so keep a coherent build system and environment is a best practice.

Distinti Saluti / Best Regards

--

Marco Cavallini | KOAN sas | Bergamo - Italia

Yocto Project Advocate

0 件の賞賛
返信

1,700件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

please look at

FSL Community BSP Release Notes 1.6 documentation

FSL Community BSP Release Notes 1.7 documentation

and post additional questions on

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信