Android usb string descriptors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android usb string descriptors

2,124 Views
chandrashekarbs
Contributor I

Hi ,

            I am using imx6qdl sabresd board. When i connect the board to windows machine it is being detected as IMX6Q-SABRESD device in device manager. How to change that string to custom name?

Please help me . Thanks in advance.

Tags (1)
0 Kudos
Reply
3 Replies

1,973 Views
chandrashekarbs
Contributor I

Hi igor,

           Thanks for the quick response.

We are trying to change the name of the board which is connected to windows machine, not the VID and PID.

Is it possible?

Regards

Chandra

0 Kudos
Reply

1,973 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

1,973 Views
igorpadykov
NXP Employee
NXP Employee

Hi chandra

windows machine uses VID@PID values provided by i.MX6Q ROM,

they are programmed in fuses USB_VID[31:0], USB_PID[31:0]

described in Table 5-10. Fusemap Descriptions i.MX6DQ RM

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Seems there is no way to change them as they are burned in factory.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply