Android on IMX7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android on IMX7

1,526件の閲覧回数
mehulshah
Contributor III

Hi ,

I want to port Android-M or Android-N on sabre Imx7 board . can anyone tell from where i can download the code for either

Android-M or Android-N for the same ? .

Regards,

mehul

0 件の賞賛
返信
1 返信

1,116件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi mehul,

Regarding Android M (6.0.1_2.1.0) for i.MX7, you could follow the download and compile instructions included on the IMX6_M6.0.1_2.1.0 Android Documentation, available for download at the link below:

https://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.1.0_ANDROID_DOCS&Parent_nodeId=12654116387... 

It is mentioned that the i.MX7D SABRE board is supported. Regarding Android N, it is not available yet.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信