Android boot animation change not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android boot animation change not working

3,266 Views
aravinthkumarja
Senior Contributor II

I'm using Android 9 iMX8M, HDMI display.

I have programmed to add bootanimation.zip to <OUTDIR>/system/media/

After compilation file present in above mentioned directory, but while booting screen is black No animation also my image also not shows.

 

Can you please help to fix.?

0 Kudos
Reply
4 Replies

2,961 Views
embdev1
Contributor I

Hi aravinthkumarja,

Please share the solution here if you have resolved this issue.

0 Kudos
Reply

2,944 Views
aravinthkumarja
Senior Contributor II

Check and the image size and resolution. If it more from expected then it won't show. lesser will be shown always.

0 Kudos
Reply

3,250 Views
aravinthkumarja
Senior Contributor II

Above thread has option push from outside. But I want inside the build. Can you share how to do that.

0 Kudos
Reply

3,259 Views
b36401
NXP Employee
NXP Employee
0 Kudos
Reply