Android boot animation change not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android boot animation change not working

4,378件の閲覧回数
aravinthkumarja
Senior Contributor II

I'm using Android 9 iMX8M, HDMI display.

I have programmed to add bootanimation.zip to <OUTDIR>/system/media/

After compilation file present in above mentioned directory, but while booting screen is black No animation also my image also not shows.

 

Can you please help to fix.?

タグ(3)
0 件の賞賛
返信
4 返答(返信)

4,073件の閲覧回数
embdev1
Contributor I

Hi aravinthkumarja,

Please share the solution here if you have resolved this issue.

0 件の賞賛
返信

4,056件の閲覧回数
aravinthkumarja
Senior Contributor II

Check and the image size and resolution. If it more from expected then it won't show. lesser will be shown always.

0 件の賞賛
返信

4,362件の閲覧回数
aravinthkumarja
Senior Contributor II

Above thread has option push from outside. But I want inside the build. Can you share how to do that.

0 件の賞賛
返信

4,371件の閲覧回数
b36401
NXP Employee
NXP Employee
0 件の賞賛
返信