Android boot animation change not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android boot animation change not working

3,207 次查看
aravinthkumarja
Senior Contributor II

I'm using Android 9 iMX8M, HDMI display.

I have programmed to add bootanimation.zip to <OUTDIR>/system/media/

After compilation file present in above mentioned directory, but while booting screen is black No animation also my image also not shows.

 

Can you please help to fix.?

标记 (3)
0 项奖励
回复
4 回复数

2,902 次查看
embdev1
Contributor I

Hi aravinthkumarja,

Please share the solution here if you have resolved this issue.

0 项奖励
回复

2,885 次查看
aravinthkumarja
Senior Contributor II

Check and the image size and resolution. If it more from expected then it won't show. lesser will be shown always.

0 项奖励
回复

3,191 次查看
aravinthkumarja
Senior Contributor II

Above thread has option push from outside. But I want inside the build. Can you share how to do that.

0 项奖励
回复

3,200 次查看
b36401
NXP Employee
NXP Employee
0 项奖励
回复