Android Verified Boot 2.0 support on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Verified Boot 2.0 support on imx6

1,652 Views
prasannakulkarni
Contributor IV

Hi,

We are using imx6dl which runs on Android 8.0.0 Oreo and Linux kernel 4.9.17. My doubt is, in this release Android Verified Boot 2.0 support is available or not?

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prasanna

supported functionalities are described in Release Notes, included

in Android O8.0.0_1.0.0  Documentation

Seems it is not supported, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply