Android Verified Boot 2.0 support on imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Verified Boot 2.0 support on imx6

1,651件の閲覧回数
prasannakulkarni
Contributor IV

Hi,

We are using imx6dl which runs on Android 8.0.0 Oreo and Linux kernel 4.9.17. My doubt is, in this release Android Verified Boot 2.0 support is available or not?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,605件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prasanna

supported functionalities are described in Release Notes, included

in Android O8.0.0_1.0.0  Documentation

Seems it is not supported, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信