Android Source Code Download for IMX processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Source Code Download for IMX processor

2,423件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

I am working in Android porting on imx6 processor for download the android source code I am following the "Android_User_Guide,pdf". 

3.1 Getting i.MX Android release source code
The i.MX Android release source code consists of three parts:
• NXP i.MX public source code, which is maintained in the CodeAurora Forum repository.
• AOSP Android public source code, which is maintained in android.googlesource.com.
• NXP i.MX Android proprietary source code package, which is maintained in www.NXP.com

For Developing the BSP which one I want to download for imx6 processor.

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(3)
0 件の賞賛
返信
1 返信

2,049件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  in general all sources may be needed for BSP development.

Also, the following may be helpful:

https://groups.google.com/forum/#!topic/android-porting/3pmtvr1kgi4


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信