Android SD Boot (imx6DL) : Binder Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android SD Boot (imx6DL) : Binder Error

6,233件の閲覧回数
sreeharshap
Contributor II

BinderError.pngHello there,

Facing the problem of BINDER ERROR. I followed instruction provide in "Android User's Guide" to build and download to SD card. When I boot with SD card, I get continuous "binder: 194:194 transaction failed 29189, size 0-0" message  and doesn't move further. Please let me know what has to be done to get rid of this issue. 

Thanks

ラベル(1)
0 件の賞賛
返信
10 返答(返信)

5,740件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreeharsha

one can try to debug it in common/drivers/staging/android/binder.c

also please check binder issue on

android booting problem with binder issue on imx6 sabrelite 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,740件の閲覧回数
sreeharshap
Contributor II

Hello Igor,

Thanks for the quick update.

Also when I use "fsl-sdcard-partition.sh", I get this following message about partition

- /dev/sdb5 is not a block special device

proceed anyway? (y,n).

It means, I'm unable to create /dev/sdb5 partition to write system.img.

Can you please help to create this partition?

Thanks

0 件の賞賛
返信

5,740件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

what BSP used in the case ?

Best regards
igor

0 件の賞賛
返信

5,740件の閲覧回数
sreeharshap
Contributor II

Hi,

m6.0.1_2.1.0.0-ga

Thanks

0 件の賞賛
返信

5,740件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi Sreeharsha,

Can you attach full log.

<i think it is unable to file system image>

Regards,

Aravinth

0 件の賞賛
返信

5,738件の閲覧回数
sreeharshap
Contributor II

Hi Aravith,

I have attached the boot log. please have a look.

Even with the pre-build I'm getting the same error.

Thanks

0 件の賞賛
返信

5,738件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi Sreeharsha,

System image is not   mounted.

This is my log:

Below 2 line is not coming in your log.

EXT4-fs (mmcblk3p5): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/mmcblk3p5,target=/system,type=ext4)=0
EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=0
EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=0
EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=0
init: Starting service 'logd'...

In your log:

mmc2: new high speed SDHC card at address aaaa
mmcblk2: mmc2:aaaa SS08G 7.40 GiB
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
mmcblk2: p4 size 13312000 extends beyond EOD, truncated

Can you check why it is coming??

Hope above information is helpful for you!

Regards,

Aravinth

0 件の賞賛
返信

5,738件の閲覧回数
sreeharshap
Contributor II

Hi Aravinth,

Thank you so much for the update. It was helpful but I still face same issue.

Unable to find a way out. The issue happens with both M6.0.1_2.1.0.4.1 pre-build and as well as locally compiled images.

When I use L5.0.0_1.0.1 pre-build, it works fine.

If you don't mind, is it possible to provide a SD image for my locally complied images?

1. I have uploaded the Images following url (password : T2NXPC1910)

https://storage.tomen-ele.co.jp/public/4OwkgACHcggA_noBZWxXXKbb7Xi1czfPG_b8ekg6vWWZ

2. In the zip, you have

boot-imx6dl.img

recovery-imx6dl.img

system.img

u-boot-imx6dl.imx

3. If it's not a issue for you, please verify images by writing to SD and booting with it.

4. If it works fine, please provide the SD image using tools like Win32DiskImager (you can upload the image to following URL).

https://storage.tomen-ele.co.jp/public/sOyAgAhHkogAMpEBLthXilnbeyG4g8cKm4wVAru5YR1W

Looking forward to your update.

Thanks

Harsha.

0 件の賞賛
返信

5,738件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi Harsha,

I'm using custom board. In this no SD-card, i'm using EMMC boot mode only.

Can you try with emmc flash.

Regards,

Aravinth

0 件の賞賛
返信

5,738件の閲覧回数
sreeharshap
Contributor II

Hello Aravintha,

I'll try that but actually our target is SD.

Anyway, please let me know if you get any other hint on your side.

Thanks

Harsha

Sent from my iPhone

0 件の賞賛
返信