Android Runtime engine on Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Runtime engine on Linux

2,470件の閲覧回数
sandeshd
Contributor I

Hi,

We are working on Android apps install and execute on Linux platform, where we would like to bringup Android Runtime Engine(RTE) on Linux platform. if anyone tried the Android RTE on Linux platform:

-  we need to install and execute android third party apps on Android RTE,, what the changes we need to do w.r.t Linux platform.

-  we need to execute Android RTE on background layer in Linux UI.

- How we can access Linux resources like local data storage, network storage and other Linux system resources .

- Access Linux BSP and multimedia functionalities from Android RTE.

- Any changes related to Graphics driver.

- Do we need to modify any changes in Android RTE if any third party requires new system resources.

- Does this effect the system performance.

- Generally Android on i.MX6 takes > 30 seconds booting time, if we bringup Android RTE on Linux platform, what is the system booting time.

It will helpful for us to understand the Android RTE on Linux platform.

thanks,

Sandesh D

ラベル(4)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,001件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello Sandesh D,

Thank you for writing.

Giving this case, we recommend you to use our Android BSP image. Because, if you want to execute Android Run Time in a Linux platform, is going to take you a lot of time and is going to be laborious.

Best Regards,

Diego.

0 件の賞賛
返信

2,001件の閲覧回数
sandeshd
Contributor I

Thanks Diego for your response.

0 件の賞賛
返信