Question, i.MX6SX CAN FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6SX CAN FIFO

Jump to solution
1,548 Views
SLICE
Contributor IV

Dear team,

My customer saw that sometimes i.MX6SX cannot receive CAN data from external.

The phenomenon could occur on MCIMX6SX-SDB with Yocto 4.1.15_1.1.0.

The customer believes that i.MX6SX has 6bytes of RX FIFO buffer and it needs to be exceeded.

Could you show me how to increase the RX FIFO?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
1,454 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

RX FIFO is 6-deep defined by hardware and can not be changed by software,

according to sect.27.1.1 Block Diagram, sect.27.1.2 FLEXCAN Module Features i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,455 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

RX FIFO is 6-deep defined by hardware and can not be changed by software,

according to sect.27.1.1 Block Diagram, sect.27.1.2 FLEXCAN Module Features i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply