Android M6 on IMX6 Freeze Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android M6 on IMX6 Freeze Issue

ソリューションへジャンプ
2,752件の閲覧回数
kirangv
Contributor III

Hello,

 

I am working with i.MX 6Quad SABRE-AI board and I tried to flash board image and boot from SD card.

I have followed "android_M6.0.1_2.1.0_docs/Android_Quick_Start_Guide" section 4.3.

 

I have successfully flashed and booted from SD card , but with in a minute the board goes into a freeze state. 

Please find the attached crash log for more details.

 

Please guide me on this.android m6.0

 

Thanks,

Kiran

Original Attachment has been moved to: Android_crash_log.txt.zip

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,396件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

you need to go into the 'settings' to change the time of suspend, default is 1 min.  

元の投稿で解決策を見る

3 返答(返信)
2,396件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Seems it entered to the suspend mode. please press the button on the base board to resume.

2,396件の閲覧回数
kirangv
Contributor III

Thank you for the reply.

I have pressed SW5 button on the base board to get the board to resume , but again it goes into suspend mode soon.

-------------------------------------------------------------------------------------------------------------------------------------------

root@sabreauto_6q:/ #
root@sabreauto_6q:/ #
root@sabreauto_6q:/ # mma enable setting inactive
PM: suspend entry 1970-01-01 00:08:20.725925005 UTC
type=1400 audit(500.720:33): avc: denied { unlink } for pid=532 comm="android.bg" name="screen_on_time.bak" dev="mmcblk2p4" ino=234400 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0
PM: Syncing filesystems ... done.
Freezing user space processes ...
PM: Wakeup pending, aborting suspend
active wakeup source: PowerManagerService.Broadcasts

Freezing of tasks aborted after 0.008 seconds
Restarting tasks ... done.
PM: suspend exit 1970-01-01 00:08:20.794502005 UTC
PM: suspend entry 1970-01-01 00:08:20.899686671 UTC
PM: Syncing filesystems ... done.
Freezing user space processes ... (elapsed 0.001 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
Suspending console(s) (use no_console_suspend to debug)
PM: suspend of devices complete after 46.711 msecs
PM: suspend devices took 0.050 seconds
PM: late suspend of devices complete after 1.069 msecs
PM: noirq suspend of devices complete after 1.079 msecs
Disabling non-boot CPUs ...
CPU1: shutdown
CPU2: shutdown
CPU3: shutdown
Resume caused by IRQ 61
Resume caused by IRQ 100
Suspended for 0.000 seconds
Enabling non-boot CPUs ...
CPU1 is up
CPU2 is up
CPU3 is up
PM: noirq resume of devices complete after 0.960 msecs
PM: early resume of devices complete after 0.609 msecs
PM: resume of devices complete after 131.081 msecs
PM: resume devices took 0.130 seconds
Restarting tasks ... done.
PM: suspend exit 1970-01-01 00:08:37.133482333 UTC
type=1400 audit(517.160:34): avc: denied { rename } for pid=944 comm="droid.deskclock" name="com.android.deskclock_preferences.xml" dev="mmcblk2p4" ino=363790 scontext=u:r:untrusted_app:s0:c512,c768 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0
period 66 ,timeout is 0, wake up is :0
mma enable setting active

root@sabreauto_6q:/ #
root@sabreauto_6q:/ #
root@sabreauto_6q:/ # mma enable setting inactive
type=1400 audit(527.810:35): avc: denied { unlink } for pid=532 comm="android.bg" name="screen_on_time.bak" dev="mmcblk2p4" ino=234400 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=0
PM: suspend entry 1970-01-01 00:08:47.837328668 UTC
PM: Syncing filesystems ... done.
Freezing user space processes ...
PM: Wakeup pending, aborting suspend
active wakeup source: PowerManagerService.Broadcasts

Freezing of tasks aborted after 0.008 seconds
Restarting tasks ... done.
PM: suspend exit 1970-01-01 00:08:47.876956334 UTC
PM: suspend entry 1970-01-01 00:08:47.981855334 UTC
PM: Syncing filesystems ... done.
Freezing user space processes ... (elapsed 0.001 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
Suspending console(s) (use no_console_suspend to debug)

-------------------------------------------------------------------------------------------------------------------------------------------

Appreciate any help on this

0 件の賞賛
返信
2,397件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

you need to go into the 'settings' to change the time of suspend, default is 1 min.