Android Kitkat supplicant compilation error for SabreSD board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android Kitkat supplicant compilation error for SabreSD board

1,785 次查看
susangracerapak
Contributor II

Hi,

I have build the Android kitkat image for Sabre SD.

I am getting the supplicant error.Can anyone help me to fix this?

root@cpu347:/work/myandroid/external/wpa_supplicant_8/wpa_supplicant# mm
============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=4.4.3
TARGET_PRODUCT=sabresd_6dq
TARGET_BUILD_VARIANT=user
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
TARGET_CPU_VARIANT=cortex-a9
HOST_ARCH=x86
HOST_OS=linux
HOST_OS_EXTRA=Linux-3.11.0-15-generic-x86_64-with-Ubuntu-12.04-precise
HOST_BUILD_TYPE=release
BUILD_ID=2.0.0-rc2
OUT_DIR=out
============================================
No private recovery resources for TARGET_DEVICE sabresd_6dq
make: Entering directory `/work/myandroid'
target thumb C: wpa_supplicant <= external/wpa_supplicant_8/wpa_supplicant/src/drivers/driver_nl80211.c
target Executable: wpa_supplicant (out/target/product/sabresd_6dq/obj/EXECUTABLES/wpa_supplicant_intermediates/LINKED/wpa_supplicant)
out/target/product/sabresd_6dq/obj/EXECUTABLES/wpa_supplicant_intermediates/src/drivers/driver_nl80211.o:driver_nl80211.c:function wpa_driver_nl80211_ops: error: undefined reference to 'wpa_driver_nl80211_driver_cmd'
collect2: error: ld returned 1 exit status
make: *** [out/target/product/sabresd_6dq/obj/EXECUTABLES/wpa_supplicant_intermediates/LINKED/wpa_supplicant] Error 1
make: Leaving directory `/work/myandroid'

Regards

Susan

0 项奖励
回复
5 回复数

1,539 次查看
susangracerapak
Contributor II

Hi Aravinth,

 

I am using RS9113 Redpine Custom Wifi chipset.

 

Regards

Susan

0 项奖励
回复

1,539 次查看
susangracerapak
Contributor II

Hi Aravinth,

I am using RS9113 Redpine Customer Wifi chip.

Regards

Susan

0 项奖励
回复

1,539 次查看
susangracerapak
Contributor II

Hi Aravinth,

I have build the complete Android BSP with the help of Android User Guide.

Do you have any idea about this issue?

Regards

Susan

0 项奖励
回复

1,539 次查看
aravinthkumarja
Senior Contributor II

Hi Susan,

Can you tell me which WiFi chip you are using.?

Regards,

Aravinth

0 项奖励
回复

1,539 次查看
aravinthkumarja
Senior Contributor II

Hi Susan,

Have you build entire Android BSP.?

Regards,

Aravinth

0 项奖励
回复