[Android] IPU error when system is too hot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Android] IPU error when system is too hot

ソリューションへジャンプ
9,923件の閲覧回数
charleshuang
Senior Contributor II

Hi,

We have an issue about IPU error, when we try to play two 1080p videos at the same time on i.MX6 Android product.

[Reproduce steps]

1. Play two 1080p @ 30fps videos with Uptmate APK.

2. Check the temperature on the device.

[Symptom]

When the temperature is over system hot limitation (90 C), it starts to downgrade GPU & CPU working frequency.

However, IPU error is coming subsequently.

Then, the screen is blocked. Framebuffer cannot be updated anymore.


[Kernel log]

System is too hot. GPU3D will work at 1/64 clock.

thermal_notify: trip_hot reached!

cooling: cpu cur freq is 996000000

cooling: cpu max freq set to 792000000

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00080000

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00800000

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

[Expected result]

We think the thermal protect mechanism should not cause IPU crashed.

Please help to investigate this issue.

Thanks,

Daniel

ラベル(4)
1 解決策
4,952件の閲覧回数
danielhung
Contributor III

Chris, thank you!

Althought I fail to patch the GPU 12 on Android 4.2.2_1.0.0, this issue can be solved by setting the minimum GPU clock to 3.

I only apply the following patch from BSP 1.1.0.

5716-ENGR00265465-gpu-Add-global-value-for-minimum-3D-clo.patch

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,952件の閲覧回数
giorgiosoldavin
Contributor I

Hi There,

I have probabily the same probleme (get IO_PAN_DISPLAY error) on my ARM6S board with Android 4.0.4.. Please, is there any patch for my environment?

Thank you for your support.

Kind regards,

Giorgio

0 件の賞賛
返信
4,952件の閲覧回数
danielhung
Contributor III

Hi,

We have some updates for this issue.

1. The thermal protect mechanism seems not the root cause for IPU error.

=> We decrease the thermal system hot criteria from 90 C to 60 C, and find video playback still works well when the thermal protect mechanism is starting.

     Therefore, the IPU error seems caused by ambient high temperature.

2. We also measure the surface temperature by temperature meter on CPU. When the issue happens, it can reach over 100 degrees centigrade.

    By cat /sys/class/thermal/thermal_zone0/temp, it also reads about 90 degrees centigrade.

Best regards,

Daniel

0 件の賞賛
返信
4,952件の閲覧回数
Chris1z
Contributor III

We have also seen this running 4.2.2-1.1.0-ga release of Android.  I found that once we upgraded GPU code, there was a new sysfs you can use to set the minimum GPU clock.  Changing from (1/64) to (3/64) has prevented the "timeout when waiting for flip irq" issue from happening.

GPU 12 code:

https://community.freescale.com/docs/DOC-99217

Add this to init script to change min GPU clock:

write /sys/module/galcore/parameters/gpu3DMinClock 3

4,953件の閲覧回数
danielhung
Contributor III

Chris, thank you!

Althought I fail to patch the GPU 12 on Android 4.2.2_1.0.0, this issue can be solved by setting the minimum GPU clock to 3.

I only apply the following patch from BSP 1.1.0.

5716-ENGR00265465-gpu-Add-global-value-for-minimum-3D-clo.patch

0 件の賞賛
返信