Android Factory Reset Issue: Android 11, imx8q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android Factory Reset Issue: Android 11, imx8q

5,812 次查看
MrNate
Contributor I

I'm using the Android 11 delivery for the imx8q and am coming across the following scenario that is giving me a terrible time.  This was tested with the stock Android build with no local changes.  Any thoughts where to look to fix this?

Success path

1.  Flash an A11 build

2.  Do a factory reset <--success

Failure Path

1. Flash A11 build

2.  Do an OTA update

3.  Do a factory reset <-- failure

Error Log:

[  323.210779] -- Wiping data...
[  323.231008] I:[libfs_mgr]superblock s_max_mnt_count:65535,/dev/block/by-name/metadata
[  323.264835] I:[libfs_mgr]check_fs(): mount(/dev/block/by-name/metadata,/metadata,ext4)=0: Success
[  323.274898] I:[libfs_mgr]check_fs(): unmount(/metadata) succeeded
[  323.275033] I:[libfs_mgr]Not running /system/bin/e2fsck on /dev/block/mmcblk0p11 (executable not in system image)
[  323.321064] I:[libfs_mgr]__mount(source=/dev/block/by-name/metadata,target=/metadata,type=ext4)=0: Success
[  323.322758] I:Creating logical partitions with snapshots as needed
[  323.361040] I:[libfs_mgr]Created logical partition system_b-base on device /dev/block/dm-5
[  323.389060] I:[libfs_mgr]Created logical partition system_b-cow-img on device /dev/block/dm-6
[  323.401994] I:Mapped system_b-cow-img to 254:6
[  323.405555] E:DM_DEV_CREATE failed for [system_b-cow]: Device or resource busy
[  323.427629] E:Could not create COW device: system_b-cow
[  323.549046] E:Unable to map partitions to complete merge.
[  323.605258] Unable to check merge status and/or complete update merge.
[  323.644265] Unable to check update status or complete merge, cannot wipe partitions. 

标记 (1)
0 项奖励
回复
3 回复数

5,738 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the full Android version that you're working with?
Also, is it standard Android or is it Android Auto?

Best regards,
Aldo.

0 项奖励
回复

5,731 次查看
MrNate
Contributor I

@AldoG 

 

 Android Auto.  11.0.0_1.1.0 

Thanks for looking into this.

Preliminary look makes it seem this is also happening on 2.5.0

0 项奖励
回复

5,716 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Thank you for sharing more information, could you try with what was proposed by google here:
https://source.android.com/docs/core/ota/virtual_ab/implement-patches#fix-slot-switch

Best regards,
Aldo.

0 项奖励
回复