Dear NXP,
I am working on iMX8 with Android P Automotive. I confused with value mentioned in the following file.
Could you explain the following content (mentioned in bold) and let me know for adding new parameter and adding values.
source/vendor/nxp-opensource/kernel_imx/drivers/mxc/vehicle/vehicle_core.h
#ifdef CONFIG_VEHICLE_DRIVER_OREO
#define HVAC_FAN_SPEED 306185472
#define HVAC_FAN_DIRECTION 306185473
#define HVAC_AUTO_ON 304088330
#define HVAC_AC_ON 304088325
#define HVAC_RECIRC_ON 304088328
#define HVAC_DEFROSTER 320865540
#define HVAC_TEMPERATURE_SET 308282627
#define HVAC_POWER_ON 304088336
#else
#define HVAC_FAN_SPEED 356517120
#define HVAC_FAN_DIRECTION 356517121
#define HVAC_AUTO_ON 354419978
#define HVAC_AC_ON 354419973
#define HVAC_RECIRC_ON 354419976
#define HVAC_DEFROSTER 320865540
#define HVAC_TEMPERATURE_SET 358614275
#define HVAC_POWER_ON 354419984
#endif
Thanks & Regards,
VinothS
已解决! 转到解答。
This is the problem with emulator. I closed this thread now.
Regards,
VinothS
Hi vinothkumars,
I went through vehicle Hal, It says vehicle HAL is connected to an emulator instead of a real vehicle network. I dont see any implementations wrt to communication with CAN.
Is there a way Vehicle HAL can receive CAN commands and send it up to application? I want this in cortex A35 .I dont want to move can to M4. I have tested CAN on IMX8 using canutils.
Regards,
Sriraksha
Hi vinothkumars,
Physical CAN communicate with Vehicle HAL via Emulator only and the Callbacks called by CAR service from Emulator.
Could you be elaborate or give more insight into this?
I went through the code but couldn't find any code related to CAN communication with HAL via Emulator.
I also saw your post on sending CAN data to HAL. How are you sending this?
Problem in sending Int array vehicle data
Regards,
Sriraksha
Hi vinothkumars,
Thank you. I wanted to try without porting can to M4. Isn't it possible in cortex a35?
I was thinking as canutils talk to can driver and dump messages cant I do the same dumping & sending it to vhal?
I am want to send dummy data from VHAL to car services up to application?
Any examples or pointers to this?
Regards,
Sriraksha
Hi,
By default CAN communication needs M4 MCU (rpmsg)
Check dts file,
source/vendor/nxp-opensource/kernel_imx/arch/arm64/boot/dts/freescale
You can use dumpsys commands to simulation purpose,
Regards,
VinothS,
Hi vinothkumars
Thank you.
Any idea on when will default implementation ie vehicle emulator called ? /hardware/interfaces/automotive/vehicle/2.0/default/impl/vhal_v2_0/
I have manually started the service./vendor/bin/hw/android.hardware.automotive.vehicle@2.0-service Logs as below: 05-14 09:06:03.348 4893 4893 I VehicleEmulator_v2_0: registerEmulator, emulator: 0xe3b636c0d380 05-14 09:06:03.349 4893 4893 I VehicleEmulator_v2_0: Starting SocketComm 05-14 09:06:03.349 4893 4893 I automotive.vehicle@2.0-impl: VehicleHalManager::init 05-14 09:06:03.351 4893 4893 I automotive.vehicle@2.0-service: Registering as service... 05-14 09:06:03.353 1772 1772 W hwservicemanager: Detected instance of android.hardware.automotive.vehicle@2.0::IVehicle (pid: 4893) registering over instance of or with base of android.hardware.automotive.vehicle@2.0::IVehicle (pid: 1901). 05-14 09:06:03.354 4893 4893 I ServiceManagement: Registered android.hardware.automotive.vehicle@2.0::IVehicle/default (start delay of 70ms) 05-14 09:06:03.354 4893 4893 I ServiceManagement: Removing namespace from process name android.hardware.automotive.vehicle@2.0-service to vehicle@2.0-service. 05-14 09:06:03.355 4893 4893 I automotive.vehicle@2.0-service: Ready I dont see any logs from SocketComm or any communication happening? Am i missing something? Regards,
Sriraksha
Hi vinothkumars,
Yes i was able to run kitchen sink app application and look into different menu like VHAL or property etc. But none of the calls were made to this vehicle emulator here /hardware/interfaces/automotive/vehicle/2.0/default/impl/vhal_v2_0/. I dint see any logs from vehicle service
(/vendor/bin/hw/android.hardware.automotive.vehicle@2.0-service)
when Kitchen sink app is running.
Build steps:
source build/envsetup.sh
lunch mek_8q_car-userdebug
./imx-make.sh -j4
for any changes in modules i use mma.
I read that SocketComm opens a socket, and listens for connections from clients. Typically the client will be
adb's TCP port-forwarding to enable a host PC to connect to the VehicleHAL. So what basically is it reading from adb? 
I am getting confused here.Currently SocketComm thread is not started at all. I dont see any logs from it.
Regards,
Sriraksha
Hi,
for example PERF_VEHICLE_SPEED
Open the KitchenSink application -> select property tab -> enable PERF_VEHICLE_SPEED
send the following command from terminal,
dumpsys activity service com.android.car inject-vhal-event 0x11600207 23
Provide your full log also
VinothS,
Hi vinothkumars,
dumpsys activity service com.android.car inject-vhal-event 0x11600207 23
what are those numbers in the above command?
This is the log when i do a dumpsys after selecting perf_vehicle_speed
rvice com.android.car inject-vhal-event 0x11600207 23 <
SERVICE com.android.car/.CarService 902335a pid=2237
 Client:
SERVICE com.android.car/.PerUserCarService dd2644b pid=3192
 Client:
 nothing to dump
SERVICE com.android.car.hvac/.HvacController c0ac038 pid=2640
 Client:
 nothing to dump
SERVICE com.android.car.hvac/.HvacUiService d9977f9 pid=2640
 Client:
 nothing to dump
SERVICE com.android.car.messenger/.MessengerService ddd9f33 pid=3368
 Client:
 nothing to dump
i have attached complete log and screenshot as well.
   
Hi,
This the message id and it's defined in types.hal
/** 
* Speed of the vehicle 
* 
* @change_mode VehiclePropertyChangeMode:ON_CHANGE|VehiclePropertyChangeMode:CONTINUOUS 
* @access VehiclePropertyAccess:READ 
* @unit VehicleUnit:METER_PER_SEC 
*/ 
PERF_VEHICLE_SPEED = ( 
0x0207 
| VehiclePropertyGroup:SYSTEM 
| VehiclePropertyType:FLOAT | VehicleArea:GLOBAL),
0x11600207
1 -> SYSTEM = 0x10000000,
1 -> GLOBAL = 0x01000000,
60 -> FLOAT = 0x00600000,
207 -> Alternative numaber
Regards,
Vinoth S,
hi vinothkumars,
Thank you.
Did you find anything from the logs ?why there are no dumps related to vehicle speed?
Regards,
Sriraksha 
hi vinothkumars,
May I know how and where did u add new vehicle parameters?
And how did u verify the communication between M4 to CAN bus?
Regards,
Ramesh
Please find the below reference link,
Thanks & Regards,
Vinoth S,
Hi vinothkumars,
Thank you for sharing it.
How do we test the vehicle property added?
Any idea of running vehicle hal test found here
<sources>packages/services/Car/tests/vehiclehal_test
or
running emulator in
<sources>/hardware/interfaces/automotive/vehicle/2.0/default/tests
Regards,
Ramesh
We have kitchensink Application and this is the command used for launch the kitchensink application,
Path: packages/services/Car/tests/EmbeddedKitchenSinkApp
commands,
am start -n com.google.android.car.kitchensink/com.google.android.car.kitchensink.KitchenSinkActivity
Note: Check Android User Guide for build with M4 as well without M4
Thanks & Regards,
Vinoth S,
Hi yifei.ren@hirain.com ,
Could you tell me, how vehicle data flow from M4 to CAN Bus ?
And also I got error, When I send the following command,
echo 2 > /sys/devices/platform/vehicle-dummy/hvac_on
Unable to handle kernel NULL pointer dereference at virtual address 000000171
After Kernel crashed and reboot.
Thanks,
VinothS,