Android 7 Bluethooth Stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 7 Bluethooth Stack

2,867 Views
jith
Contributor II

Hi,

Which is the Bluetooth stack used in Android 7?

Is it support Bluetooth 5?

Labels (1)
2 Replies

2,585 Views
jith
Contributor II

Thank you so much

0 Kudos
Reply

2,585 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jith

as Android 7 is based on L4.1.15 kernel one can refer to

sect.55.3.3 Bluetooth Stack attached Linux Manual

Android N7.1.1_1.0.0 Release Announcement 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------