Android 7.1.2 MFG-tool image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 7.1.2 MFG-tool image

Jump to solution
1,764 Views
xiezhiyong
Senior Contributor II

Our product is using imx6qplus and Android 7.1.2.

We want to do eMMC boot.

We use "mfgtoolsL4.9.11_1.0.0" to write eMMC ,but follow  error log is come out.

########################

Wrong Ramdisk Image Format

Ramdisk image is corrupt or invalid

########################

Do the file "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" can't be used directly?

How to fix this problem?

Labels (1)
0 Kudos
Reply
1 Solution
1,663 Views
xiezhiyong
Senior Contributor II

I check config about conig of u-boot .CONFIG_ENV_IS_NOWHERE isn't defined.

I define this config and build u-boot.imx again.

The Ramdisk image can be loaded.

View solution in original post

0 Kudos
Reply
1 Reply
1,664 Views
xiezhiyong
Senior Contributor II

I check config about conig of u-boot .CONFIG_ENV_IS_NOWHERE isn't defined.

I define this config and build u-boot.imx again.

The Ramdisk image can be loaded.

0 Kudos
Reply