Android 6 reboot error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 6 reboot error

2,664件の閲覧回数
julianmp
Contributor II

I compile android with the flag build_device_target=sd, the first boot all goes well but if i reboot or shutdown i have the following errors in partitions, I attach the log, How can I solve it?

U-Boot SPL 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)

SPL: u-boot second stage will be loaded from MMC0

U-Boot 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)


CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 38 C

Reset cause: WDOG

Board: UDOO Quad

       Watchdog enabled

DRAM:  1 GiB

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment


auto-detected panel HDMI

Display: HDMI (1280x720)

In:    serial

Out:   serial

Err:   serial

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:0

Net:   using phy at 6

FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  3     2     1     0

112 bytes read in 148 ms (0 Bytes/s)

Running bootscript from mmc ...

Device Tree: dts/imx6q-udoo-hdmi.dtb

42833 bytes read in 86 ms (486.3 KiB/s)

boota mmc0

kernel   @ 14008000 (5719992)

ramdisk  @ 15000000 (917604)

fdt      @ 14f00000 (42833)

## Booting Android Image at 0x12000000 ...

Kernel load addr 0x14008000 size 5586 KiB

Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend

## Flattened Device Tree blob at 14f00000

   Booting using the fdt blob at 0x14f00000

   Loading Kernel Image ... OK

   Using Device Tree in place at 14f00000, end 14f0d750


Starting kernel ...


[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 3.14.52-09424-g6fe6e7b-dirty (root@eyenai-VirtualBox) (gcc version 5.3.1 20160401 (optimized) (UBERTC-5.3.x) ) #1 SMP PREEMPT Wed Feb 7 21:19:47 CET 2018
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: UDOO Quad Board
[    0.000000] cma: CMA: reserved 256 MiB at 2e000000
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] PERCPU: Embedded 8 pages/cpu @ee741000 s8640 r8192 d15936 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260384
[    0.000000] Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend androidboot.serialno=0c09a1d4e3173fe7  
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 763932K/1047552K available (7132K kernel code, 439K rwdata, 2408K rodata, 288K init, 497K bss, 283620K reserved, 277504K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xef800000 - 0xff000000   ( 248 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xef000000   ( 752 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0959514   (9542 kB)
[    0.000000]       .init : 0xc095a000 - 0xc09a21c0   ( 289 kB)
[    0.000000]       .data : 0xc09a4000 - 0xc0a11d80   ( 440 kB)
[    0.000000]        .bss : 0xc0a11d8c - 0xc0a8e400   ( 498 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] L310 cache controller enabled
[    0.000000] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB
[    0.000000] Switching to timer-based delay loop
[    0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
[    0.000816] Console: colour dummy device 80x30
[    0.000840] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[    0.000853] pid_max: default: 32768 minimum: 301
[    0.000956] Security Framework initialized
[    0.001010] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001022] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001663] Initializing cgroup subsys debug
[    0.001676] Initializing cgroup subsys freezer
[    0.001701] CPU: Testing write buffer coherency: ok
[    0.001952] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.002006] Setting up static identity map for 0x106cebc0 - 0x106cec18
[    0.060999] CPU1: Booted secondary processor
[    0.061020] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.080985] CPU2: Booted secondary processor
[    0.081005] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[    0.100984] CPU3: Booted secondary processor
[    0.101004] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[    0.101103] Brought up 4 CPUs
[    0.101132] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[    0.101141] CPU: All CPU(s) started in SVC mode.
[    0.101568] devtmpfs: initialized
[    0.105161] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.105482] pinctrl core: initialized pinctrl subsystem
[    0.105789] regulator-dummy: no parameters
[    0.120425] NET: Registered protocol family 16
[    0.128269] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.128813] cpuidle: using governor ladder
[    0.128823] cpuidle: using governor menu
[    0.129213] CPU identified as i.MX6Q, silicon rev 1.2
[    0.129339] Use WDOG1 as reset source
[    0.136255] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
[    0.136525] vdd1p1: 800 <--> 1375 mV at 1100 mV
[    0.136844] vdd3p0: 2625 <--> 3400 mV at 3000 mV
[    0.137153] vdd2p5: 2000 <--> 2750 mV at 2400 mV
[    0.137446] vddarm: 725 <--> 1450 mV at 1150 mV
[    0.140361] vddpu: 725 <--> 1450 mV
[    0.140687] vddsoc: 725 <--> 1450 mV at 1175 mV
[    0.142467] syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
[    0.144580] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
[    0.147985] apx_wdog trigger loaded
[    0.148004] apx_wdog: enabled wdog - 0 s between refresh
[    0.148884] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.148894] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.149526] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[    0.170971] bio: create slab <bio-0> at 0
[    0.172857] mxs-dma 110000.dma-apbh: initialized
[    0.173465] usb_h1_vbus: 5000 mV
[    0.173658] usb_otg_vbus: 5000 mV
[    0.173845] 2P5V: 2500 mV
[    0.174184] i2c-core: driver [max17135] using legacy suspend method
[    0.174193] i2c-core: driver [max17135] using legacy resume method
[    0.174709] SCSI subsystem initialized
[    0.175135] usbcore: registered new interface driver usbfs
[    0.175197] usbcore: registered new interface driver hub
[    0.175290] usbcore: registered new device driver usb
[    0.175411] usbphy_nop1.11 supply vcc not found, using dummy regulator
[    0.175500] usbphy_nop2.12 supply vcc not found, using dummy regulator
[    0.176640] i2c i2c-1: IMX I2C adapter registered
[    0.177441] i2c i2c-2: IMX I2C adapter registered
[    0.177551] Linux video capture interface: v2.00
[    0.177593] pps_core: LinuxPPS API ver. 1 registered
[    0.177602] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[    0.177625] PTP clock support registered
[    0.190411] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    0.210392] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    0.211479] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
[    0.211493] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
[    0.211555] MIPI CSI2 driver module loaded
[    0.211633] Advanced Linux Sound Architecture Driver Initialized.
[    0.212692] Loading modules backported from Linux version v4.1.7-0-g0c5c1f1
[    0.212701] Backport integrated by backports.git v4.1.1-1-0-g8286954
[    0.212710] Bluetooth: Core ver 2.20
[    0.212763] NET: Registered protocol family 31
[    0.212773] Bluetooth: HCI device and connection manager initialized
[    0.212788] Bluetooth: HCI socket layer initialized
[    0.212802] Bluetooth: L2CAP socket layer initialized
[    0.212835] Bluetooth: SCO socket layer initialized
[    0.213269] Switched to clocksource mxc_timer1
[    0.222379] NET: Registered protocol family 2
[    0.223192] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.223298] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.223425] TCP: Hash tables configured (established 8192 bind 8192)
[    0.223500] TCP: reno registered
[    0.223514] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.223554] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.223792] NET: Registered protocol family 1
[    0.224013] Trying to unpack rootfs image as initramfs...
[    0.277366] Freeing initrd memory: 896K (c5000000 - c50e0000)
[    0.277980] hw perfevents: enabled with ARMv7_Cortex_A9 PMU driver, 7 counters available
[    0.278712] imx_busfreq busfreq.15: DDR medium rate not supported.
[    0.279145] Bus freq driver module loaded
[    0.280340] futex hash table entries: 1024 (order: 4, 65536 bytes)
[    0.281969] bounce pool size: 64 pages
[    0.287125] VFS: Disk quotas dquot_6.5.2
[    0.287373] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.288706] NTFS driver 2.1.30 [Flags: R/W].
[    0.289150] fuse init (API version 7.22)
[    0.289543] msgmni has been set to 1463
[    0.292252] NET: Registered protocol family 38
[    0.292291] io scheduler noop registered
[    0.292301] io scheduler deadline registered
[    0.292335] io scheduler cfq registered (default)
[    0.292763] imx-weim 21b8000.weim: Driver registered.
[    0.294263] MIPI DSI driver module loaded
[    0.295305] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[    0.295335] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[    0.295423] mxc_sdc_fb fb.20: registered mxc display driver hdmi
[    0.333349] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[    0.402863] Console: switching to colour frame buffer device 240x67
[    0.442896] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[    0.443457] imx-sdma 20ec000.sdma: no event needs to be remapped
[    0.443904] imx-sdma 20ec000.sdma: loaded firmware 3.3
[    0.446417] imx-sdma 20ec000.sdma: initialized
[    0.446827] Serial: IMX driver
[    0.447191] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
[    1.294951] console [ttymxc1] enabled
[    1.295359] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
[    1.295645] serial: Freescale lpuart driver
[    1.296645] [drm] Initialized drm 1.1.0 20060810
[    1.297014] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[    1.303896] brd: module loaded
[    1.307567] loop: module loaded
[    1.308036] zram: Created 1 device(s) ...
[    1.308370] [bossac] Registering IRQ 323 for BOSSAC Arduino erase/reset operation
[    1.308596] [bossac] Created device file /dev/udoo_ard
[    1.309441] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[    1.309449] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[    1.309455] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[    1.309461] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[    1.313090] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[    1.313121] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[    1.313132] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
[    1.314905] scsi0 : ahci_platform
[    1.315164] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
[    1.317254] tun: Universal TUN/TAP device driver, 1.6
[    1.317257] tun: (C) 1999-2004 Max Krasnyansky <[email protected]>
[    1.317420] CAN device driver interface
[    1.318343] 2188000.ethernet supply phy not found, using dummy regulator
[    1.433650] pps pps0: new PPS source ptp0
[    1.479292] libphy: fec_enet_mii_bus: probed
[    1.479752] fec 2188000.ethernet eth0: registered PHC device 0
[    1.479942] PPP generic driver version 2.4.2
[    1.480132] PPP BSD Compression module registered
[    1.480135] PPP Deflate Compression module registered
[    1.480158] PPP MPPE Compression module registered
[    1.480163] NET: Registered protocol family 24
[    1.480237] usbcore: registered new interface driver asix
[    1.480295] usbcore: registered new interface driver ax88179_178a
[    1.480335] usbcore: registered new interface driver cdc_ether
[    1.480374] usbcore: registered new interface driver cdc_eem
[    1.480412] usbcore: registered new interface driver net1080
[    1.480450] usbcore: registered new interface driver cdc_subset
[    1.480487] usbcore: registered new interface driver zaurus
[    1.480563] usbcore: registered new interface driver cdc_ncm
[    1.480567] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.480571] ehci-mxc: Freescale On-Chip EHCI Host driver
[    1.480708] usbcore: registered new interface driver cdc_acm
[    1.480711] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.480767] usbcore: registered new interface driver usb-storage
[    1.480871] usbcore: registered new interface driver usbserial
[    1.480912] usbcore: registered new interface driver usbserial_generic
[    1.480945] usbserial: USB Serial support registered for generic
[    1.480980] usbcore: registered new interface driver ftdi_sio
[    1.481011] usbserial: USB Serial support registered for FTDI USB Serial Device
[    1.481051] usbcore: registered new interface driver option
[    1.481083] usbserial: USB Serial support registered for GSM modem (1-port)
[    1.481126] usbcore: registered new interface driver usb_ehset_test
[    1.481850] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[    1.489807] ci_hdrc ci_hdrc.1: doesn't support gadget
[    1.489825] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    1.489849] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[    1.503321] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    1.503516] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    1.503524] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    1.503530] usb usb1: Product: EHCI Host Controller
[    1.503535] usb usb1: Manufacturer: Linux 3.14.52-09424-g6fe6e7b-dirty ehci_hcd
[    1.503541] usb usb1: SerialNumber: ci_hdrc.1
[    1.504123] hub 1-0:1.0: USB hub found
[    1.504155] hub 1-0:1.0: 1 port detected
[    1.505078] mousedev: PS/2 mouse device common for all mice
[    1.505598] usbcore: registered new interface driver usbtouchscreen
[    1.506043] input: st1232-touchscreen as /devices/soc0/soc.0/2100000.aips-bus/21a8000.i2c/i2c-2/2-0055/input/input0
[    1.506897] snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
[    1.507176] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
[    1.507265] i2c /dev entries driver
[    1.508383] 2-003c supply DOVDD not found, using dummy regulator
[    1.508430] 2-003c supply DVDD not found, using dummy regulator
[    1.508467] 2-003c supply AVDD not found, using dummy regulator
[    1.663455] ata1: SATA link down (SStatus 0 SControl 300)
[    1.663495] ahci-imx 2200000.sata: no device found, disabling link.
[    1.663501] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[    1.698273] ov5640_read_reg:write reg error:reg=300a
[    1.698275] camera ov5640_mipi is not found
[    1.699042] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video16
[    1.699176] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video17
[    1.699447] usbcore: registered new interface driver uvcvideo
[    1.699449] USB Video Class driver (1.1.1)
[    1.699688] [UDOO power-off] Probed LVDS power.
[    1.699766] [UDOO power-off] Probed LVDS backlight.
[    1.699833] [UDOO power-off] Probed UDOO Quad/Dual.
[    1.700242] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
[    1.700545] device-mapper: uevent: version 1.0.3
[    1.700867] device-mapper: ioctl: 4.27.0-ioctl (2013-10-30) initialised: [email protected]
[    1.701226] sdhci: Secure Digital Host Controller Interface driver
[    1.701229] sdhci: Copyright(c) Pierre Ossman
[    1.701231] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.706455] mmc0: no vqmmc regulator found
[    1.706463] mmc0: no vmmc regulator found
[    1.743312] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[    1.743945] Warning: No contiguous memory is reserverd for gpu.!
[    1.743945]  
[    1.743951] Warning: Will use default value(134217728) for the reserved memory!
[    1.743951]  
[    1.743957] Galcore version 5.0.11.41671
[    1.823486] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[    1.926840] mmc0: host does not support reading read-only switch. assuming write-enable.
[    1.945914] mmc0: new high speed SDHC card at address 0007
[    1.946552] mmcblk0: mmc0:0007 SD32G 29.0 GiB
[    1.990777]  mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
[    2.001288] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[    2.001298] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[    2.007164] hub 1-1:1.0: USB hub found
[    2.011100] hub 1-1:1.0: 4 ports detected
[    2.258970] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[    2.259502] mxc_vpu 2040000.vpu: VPU initialized
[    2.333535] usb 1-1.1: new low-speed USB device number 3 using ci_hdrc
[    2.468402] usb 1-1.1: New USB device found, idVendor=0e8f, idProduct=00fb
[    2.475309] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    2.482648] usb 1-1.1: Product: USB Mouse
[    2.486679] usb 1-1.1: Manufacturer: YSTEK
[    2.507187] caam 2100000.caam: Instantiated RNG4 SH0
[    2.583528] usb 1-1.3: new high-speed USB device number 4 using ci_hdrc
[    2.731280] usb 1-1.3: New USB device found, idVendor=148f, idProduct=5370
[    2.738210] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[    2.745555] usb 1-1.3: Product: 802.11 n WLAN
[    2.749622] caam 2100000.caam: Instantiated RNG4 SH1
[    2.749631] caam 2100000.caam: device ID = 0x0a160100 (Era 4)
[    2.749638] caam 2100000.caam: job rings = 2, qi = 0
[    2.765637] usb 1-1.3: Manufacturer: Ralink
[    2.769831] usb 1-1.3: SerialNumber: 1.0
[    2.826183] caam algorithms registered in /proc/crypto
[    2.834987] caam_jr 2101000.jr0: registering rng-caam
[    2.840872] snvs-secvio 20cc000.caam-snvs: can't get snvs clock
[    2.846874] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
[    2.855172] hidraw: raw HID events driver (C) Jiri Kosina
[    2.866846] input: YSTEK USB Mouse as /devices/soc0/soc.0/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.1/1-1.1:1.0/0003:0E8F:00FB.0001/input/input1
[    2.881158] hid-generic 0003:0E8F:00FB.0001: input,hidraw0: USB HID v1.10 Mouse [YSTEK USB Mouse] on usb-ci_hdrc.1-1.1/input0
[    2.892585] usbcore: registered new interface driver usbhid
[    2.898212] usbhid: USB HID core driver
[    2.902884] ashmem: initialized
[    2.906228] logger: created 256K log 'log_main'
[    2.910917] logger: created 256K log 'log_events'
[    2.915792] logger: created 256K log 'log_radio'
[    2.920569] logger: created 256K log 'log_system'
[    2.926096] usbcore: registered new interface driver snd-usb-audio
[    2.933730] fsl-asrc 2034000.asrc: driver registered
[    3.003603] VT1613 SoC Audio Codec [ID = 5649 - 4123]
[    3.011667] imx-ac97-vt1613 sound.18: vt1613-hifi-analog <-> 2028000.ssi mapping ok
[    3.023525] imx-audio-hdmi sound-hdmi.19: hdmi-hifi <-> hdmi_audio.3 mapping ok
[    3.031643] NET: Registered protocol family 26
[    3.036121] u32 classifier
[    3.038836]     Actions configured
[    3.042246] Netfilter messages via NETLINK v0.30.
[    3.047041] nf_conntrack version 0.5.0 (16046 buckets, 64184 max)
[    3.053675] ctnetlink v0.93: registering with nfnetlink.
[    3.059476] xt_time: kernel timezone is -0000
[    3.064160] ip_tables: (C) 2000-2006 Netfilter Core Team
[    3.069645] arp_tables: (C) 2002 David S. Miller
[    3.074336] TCP: cubic registered
[    3.077660] Initializing XFRM netlink socket
[    3.082391] NET: Registered protocol family 10
[    3.087874] mip6: Mobile IPv6
[    3.090882] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    3.096493] sit: IPv6 over IPv4 tunneling driver
[    3.101737] NET: Registered protocol family 17
[    3.106234] NET: Registered protocol family 15
[    3.110687] can: controller area network core (rev 20120528 abi 9)
[    3.116937] NET: Registered protocol family 29
[    3.121390] can: raw protocol (rev 20120528)
[    3.125681] can: broadcast manager protocol (rev 20120528 t)
[    3.131355] can: netlink gateway (rev 20130117) max_hops=1
[    3.137002] 8021q: 802.1Q VLAN Support v1.8
[    3.141452] Key type dns_resolver registered
[    3.145884] Bluetooth: RFCOMM TTY layer initialized
[    3.150788] Bluetooth: RFCOMM socket layer initialized
[    3.155965] Bluetooth: RFCOMM ver 1.11
[    3.159816] usbcore: registered new interface driver btusb
[    3.165388] usbcore: registered new interface driver cdc_wdm
[    3.172613] ThumbEE CPU extension supported.
[    3.177637] usb_otg_vbus: disabling
[    3.181145] regulator-dummy: disabling
[    3.185681] file system registered
[    3.189902] using random self ethernet address
[    3.194393] using random host ethernet address
[    3.198920] Number of LUNs=8
[    3.201811] Mass Storage Function, version: 2009/09/11
[    3.206985] LUN: removable file: (no medium)
[    3.211471] android_usb gadget: android_usb ready
[    3.216419] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:05:55 UTC (355)
[    3.233513] ALSA device list:
[    3.236497]   #0: vt1613-audio
[    3.239556]   #1: imx-hdmi-soc
[    3.243193] Freeing unused kernel memory: 288K (c095a000 - c09a2000)
[    3.252013] init: init started!
[    3.257131] init: init second stage started!
[    3.262021] init: waitpid failed: No child processes
[    3.267190] init: property_set("ro.zygote", "zygote32") failed
[    3.273255] init: (Loading properties from /default.prop took 0.01s.)
[    3.281847] init: (Parsing /init.environ.rc took 0.00s.)
[    3.287546] init: (Parsing /init.usb.rc took 0.00s.)
[    3.293565] init: (Parsing init.freescale.usb.rc took 0.00s.)
[    3.299407] init: (Parsing init.freescale.i.MX6Q.rc took 0.00s.)
[    3.305616] init: (Parsing init.bluetooth.rc took 0.00s.)
[    3.311041] init: (Parsing /init.freescale.rc took 0.02s.)
[    3.317077] init: (Parsing /init.usb.configfs.rc took 0.00s.)
[    3.322928] init: (Parsing /init.zygote32.rc took 0.00s.)
[    3.328505] init: (Parsing /init.trace.rc took 0.00s.)
[    3.333680] init: (Parsing /init.rc took 0.05s.)
[    3.338477] init: Starting service 'ueventd'...
[    3.343584] init: Waiting for /dev/.coldboot_done...
[    3.345317] ueventd: ueventd started!
[    3.433611] ueventd: Coldboot took 0.09s.
[    3.443116] init: Waiting for /dev/.coldboot_done took 0.10s.
[    3.451251] init: write_file: Unable to open '/proc/sys/kernel/hung_task_timeout_secs': No such file or directory
[    3.461646] init: write_file: Unable to open '/proc/sys/kernel/sched_tunable_scaling': No such file or directory
[    3.471984] init: write_file: Unable to open '/proc/sys/kernel/sched_latency_ns': No such file or directory
[    3.481790] init: write_file: Unable to open '/proc/sys/kernel/sched_wakeup_granularity_ns': No such file or directory
[    3.492540] init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory
[    3.503322] init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
[    3.513109] init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
[    3.521692] init: Starting service 'watchdogd'...
[    3.527239] Console: switching to colour dummy device 80x30
[    3.528696] watchdogd: watchdogd started (interval 10, margin 20)!
[    3.563205] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: barrier=1
[    3.571685] fs_mgr: __mount(source=/dev/block/mmcblk0p5,target=/system,type=ext4)=0
[    3.580559] EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option
[    3.594543] JBD2: recovery failed
[    3.597940] EXT4-fs (mmcblk0p4): error loading journal
[    3.604704] fs_mgr: __mount(source=/dev/block/mmcblk0p4,target=/data,type=ext4)=-1
[    3.614124] fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk0p4 for mount /data type ext4 )
[    3.626235] EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option
[    3.639178] JBD2: recovery failed
[    3.642575] EXT4-fs (mmcblk0p6): error loading journal
[    3.649337] fs_mgr: __mount(source=/dev/block/mmcblk0p6,target=/cache,type=ext4)=-1
[    3.659317] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p6 at /cache options: nomblk_io_submit error: Invalid argument
[    3.677860] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
[    3.686026] fs_mgr: __mount(source=/dev/block/mmcblk0p7,target=/device,type=ext4)=0
[    3.693815] init: fs_mgr_mount_all returned an error
[    3.699009] init: fs_mgr_mount_all returned unexpected error 255
[    3.708275] init: Starting service 'logd'...
[    3.912655] random: mkswap urandom read with 29 bits of entropy available
[    3.918057] logd.auditd: start
[    3.918093] logd.klogd: 3914816666
[    3.927042] Adding 307196k swap on /dev/block/zram0.  Priority:-1 extents:1 across:307196k SS
[    3.947568] init: (Loading properties from /system/build.prop took 0.01s.)
[    3.954566] init: (Loading properties from /vendor/build.prop took 0.00s.)
[    3.961503] init: (Loading properties from /factory/factory.prop took 0.00s.)
[    3.971179] init: Starting service 'vold'...
[    3.976115] init: Not bootcharting.
[    3.981172] init: Failed to reload policy
[    3.985534] init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...
[    4.013159] init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 186) exited with status 0
[    4.022138] init: (Loading properties from /data/local.prop took 0.00s.)
[    4.029015] init: Starting service 'logd-reinit'...
[    4.037190] init: Starting service 'healthd'...
[    4.042284] init: Starting service 'console'...
[    4.045552] binder: 192:192 transaction failed 29189, size 0-0
  >ù›[    4.054696] init: Starting service 'servicemanager'...
[    4.060475] init: Starting service 'surfaceflinger'...
[    4.060502] logd.daemon: reinit
[    4.104520] init: Starting service 'daemonsu'...
[    4.109750] init: Service 'logd-reinit' (pid 189) exited with status 0
[    4.116897] init: Starting service 'exec 1 (/system/bin/fakerclocal)'...
root@udoo_6dq:/ # [    4.156899] warning: `daemonsu' uses 32-bit capabilities (legacy support in use)
[    4.167149] init: Service 'daemonsu' (pid 211) exited with status 0
[    4.349582] init: Service 'exec 1 (/system/bin/fakerclocal)' (pid 217) exited with status 0
[    4.387282] cfg80211: Calling CRDA to update world regulatory domain
[    4.393855] cfg80211: World regulatory domain updated:
[    4.399005] cfg80211:  DFS Master region: unset
[    4.403392] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[    4.413153] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[    4.421205] cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    4.430626] cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[    4.438711] cfg80211:   (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    4.448250] cfg80211:   (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[    4.457768] cfg80211:   (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[    4.465921] cfg80211:   (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[    4.473977] cfg80211:   (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[    4.518079] init: property_set("ro.ril.wake_lock_timeout", "300") failed
[    4.525553] init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
[    4.534839] init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
[    4.545167] init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
[    4.556188] init: Starting service 'disableadk'...
[    4.578073] init: Service 'disableadk' (pid 248) exited with status 0
[    5.046695] healthd: No charger supplies found
[    5.051210] healthd: No battery devices found
[    5.302461] init: Starting service 'bootanim'...
[    9.076787] random: nonblocking pool is initialized
[   16.085963] usb 1-1.1: USB disconnect, device number 3
random: nonblocking pool is initialized

/system/bin/sh: random:: not found
127|root@udoo_6dq:/ #

127|root@udoo_6dq:/ # reboot

[   92.092267] imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!
[   92.098742] reboot: Restarting system with command ''


U-Boot SPL 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)

SPL: u-boot second stage will be loaded from MMC0

U-Boot 2015.04-gbff0827 (Feb 07 2018 - 21:21:22)


CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 40 C

Reset cause: WDOG

Board: UDOO Quad

       Watchdog enabled

DRAM:  1 GiB

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment


auto-detected panel HDMI

Display: HDMI (1280x720)

In:    serial

Out:   serial

Err:   serial

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:0

Net:   using phy at 6

FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  3     2     1     0

112 bytes read in 148 ms (0 Bytes/s)

Running bootscript from mmc ...

Device Tree: dts/imx6q-udoo-hdmi.dtb

42833 bytes read in 86 ms (486.3 KiB/s)

boota mmc0

kernel   @ 14008000 (5719992)

ramdisk  @ 15000000 (917604)

fdt      @ 14f00000 (42833)

## Booting Android Image at 0x12000000 ...

Kernel load addr 0x14008000 size 5586 KiB

Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend

## Flattened Device Tree blob at 14f00000

   Booting using the fdt blob at 0x14f00000

   Loading Kernel Image ... OK

   Using Device Tree in place at 14f00000, end 14f0d750


Starting kernel ...


[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 3.14.52-09424-g6fe6e7b-dirty (root@eyenai-VirtualBox) (gcc version 5.3.1 20160401 (optimized) (UBERTC-5.3.x) ) #1 SMP PREEMPT Wed Feb 7 21:19:47 CET 2018
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: UDOO Quad Board
[    0.000000] cma: CMA: reserved 256 MiB at 2e000000
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] PERCPU: Embedded 8 pages/cpu @ee741000 s8640 r8192 d15936 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260384
[    0.000000] Kernel command line: console=ttymxc1,115200 init=/init vmalloc=256M androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=256M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend androidboot.serialno=0c09a1d4e3173fe7  
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 763932K/1047552K available (7132K kernel code, 439K rwdata, 2408K rodata, 288K init, 497K bss, 283620K reserved, 277504K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xef800000 - 0xff000000   ( 248 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xef000000   ( 752 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0959514   (9542 kB)
[    0.000000]       .init : 0xc095a000 - 0xc09a21c0   ( 289 kB)
[    0.000000]       .data : 0xc09a4000 - 0xc0a11d80   ( 440 kB)
[    0.000000]        .bss : 0xc0a11d8c - 0xc0a8e400   ( 498 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] L310 cache controller enabled
[    0.000000] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB
[    0.000000] Switching to timer-based delay loop
[    0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
[    0.000815] Console: colour dummy device 80x30
[    0.000838] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[    0.000851] pid_max: default: 32768 minimum: 301
[    0.000957] Security Framework initialized
[    0.001011] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001024] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001670] Initializing cgroup subsys debug
[    0.001683] Initializing cgroup subsys freezer
[    0.001709] CPU: Testing write buffer coherency: ok
[    0.001958] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.002010] Setting up static identity map for 0x106cebc0 - 0x106cec18
[    0.061004] CPU1: Booted secondary processor
[    0.061023] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.080987] CPU2: Booted secondary processor
[    0.081007] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[    0.100988] CPU3: Booted secondary processor
[    0.101009] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[    0.101111] Brought up 4 CPUs
[    0.101139] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[    0.101148] CPU: All CPU(s) started in SVC mode.
[    0.101580] devtmpfs: initialized
[    0.105169] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.105495] pinctrl core: initialized pinctrl subsystem
[    0.105799] regulator-dummy: no parameters
[    0.119914] NET: Registered protocol family 16
[    0.127808] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.128353] cpuidle: using governor ladder
[    0.128363] cpuidle: using governor menu
[    0.128756] CPU identified as i.MX6Q, silicon rev 1.2
[    0.128878] Use WDOG1 as reset source
[    0.135781] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
[    0.136056] vdd1p1: 800 <--> 1375 mV at 1100 mV
[    0.136379] vdd3p0: 2625 <--> 3400 mV at 3000 mV
[    0.136690] vdd2p5: 2000 <--> 2750 mV at 2400 mV
[    0.136988] vddarm: 725 <--> 1450 mV at 1150 mV
[    0.140366] vddpu: 725 <--> 1450 mV
[    0.140694] vddsoc: 725 <--> 1450 mV at 1175 mV
[    0.142480] syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
[    0.144581] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
[    0.147971] apx_wdog trigger loaded
[    0.147990] apx_wdog: enabled wdog - 0 s between refresh
[    0.148866] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.148877] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.149512] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[    0.170992] bio: create slab <bio-0> at 0
[    0.172866] mxs-dma 110000.dma-apbh: initialized
[    0.173469] usb_h1_vbus: 5000 mV
[    0.173660] usb_otg_vbus: 5000 mV
[    0.173848] 2P5V: 2500 mV
[    0.174187] i2c-core: driver [max17135] using legacy suspend method
[    0.174196] i2c-core: driver [max17135] using legacy resume method
[    0.174718] SCSI subsystem initialized
[    0.175147] usbcore: registered new interface driver usbfs
[    0.175208] usbcore: registered new interface driver hub
[    0.175303] usbcore: registered new device driver usb
[    0.175428] usbphy_nop1.11 supply vcc not found, using dummy regulator
[    0.175519] usbphy_nop2.12 supply vcc not found, using dummy regulator
[    0.176647] i2c i2c-1: IMX I2C adapter registered
[    0.177443] i2c i2c-2: IMX I2C adapter registered
[    0.177553] Linux video capture interface: v2.00
[    0.177599] pps_core: LinuxPPS API ver. 1 registered
[    0.177608] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[    0.177632] PTP clock support registered
[    0.190414] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    0.210399] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    0.211453] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
[    0.211469] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
[    0.211532] MIPI CSI2 driver module loaded
[    0.211609] Advanced Linux Sound Architecture Driver Initialized.
[    0.212654] Loading modules backported from Linux version v4.1.7-0-g0c5c1f1
[    0.212663] Backport integrated by backports.git v4.1.1-1-0-g8286954
[    0.212672] Bluetooth: Core ver 2.20
[    0.212722] NET: Registered protocol family 31
[    0.212730] Bluetooth: HCI device and connection manager initialized
[    0.212745] Bluetooth: HCI socket layer initialized
[    0.212758] Bluetooth: L2CAP socket layer initialized
[    0.212792] Bluetooth: SCO socket layer initialized
[    0.213223] Switched to clocksource mxc_timer1
[    0.222282] NET: Registered protocol family 2
[    0.223093] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.223175] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.223325] TCP: Hash tables configured (established 8192 bind 8192)
[    0.223402] TCP: reno registered
[    0.223417] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.223458] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.223698] NET: Registered protocol family 1
[    0.223925] Trying to unpack rootfs image as initramfs...
[    0.277176] Freeing initrd memory: 896K (c5000000 - c50e0000)
[    0.277788] hw perfevents: enabled with ARMv7_Cortex_A9 PMU driver, 7 counters available
[    0.278545] imx_busfreq busfreq.15: DDR medium rate not supported.
[    0.278984] Bus freq driver module loaded
[    0.280168] futex hash table entries: 1024 (order: 4, 65536 bytes)
[    0.281735] bounce pool size: 64 pages
[    0.286901] VFS: Disk quotas dquot_6.5.2
[    0.287140] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.288476] NTFS driver 2.1.30 [Flags: R/W].
[    0.288911] fuse init (API version 7.22)
[    0.289311] msgmni has been set to 1463
[    0.292122] NET: Registered protocol family 38
[    0.292162] io scheduler noop registered
[    0.292172] io scheduler deadline registered
[    0.292206] io scheduler cfq registered (default)
[    0.292633] imx-weim 21b8000.weim: Driver registered.
[    0.294122] MIPI DSI driver module loaded
[    0.295159] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[    0.295188] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[    0.295275] mxc_sdc_fb fb.20: registered mxc display driver hdmi
[    0.333301] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[    0.402818] Console: switching to colour frame buffer device 240x67
[    0.442875] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[    0.443428] imx-sdma 20ec000.sdma: no event needs to be remapped
[    0.443877] imx-sdma 20ec000.sdma: loaded firmware 3.3
[    0.446381] imx-sdma 20ec000.sdma: initialized
[    0.446791] Serial: IMX driver
[    0.447151] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
[    1.294894] console [ttymxc1] enabled
[    1.295296] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
[    1.295584] serial: Freescale lpuart driver
[    1.296578] [drm] Initialized drm 1.1.0 20060810
[    1.296947] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[    1.303808] brd: module loaded
[    1.307487] loop: module loaded
[    1.307952] zram: Created 1 device(s) ...
[    1.308294] [bossac] Registering IRQ 323 for BOSSAC Arduino erase/reset operation
[    1.308516] [bossac] Created device file /dev/udoo_ard
[    1.309364] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[    1.309372] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[    1.309379] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[    1.309385] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[    1.313032] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[    1.313061] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[    1.313073] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
[    1.314776] scsi0 : ahci_platform
[    1.315038] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
[    1.317124] tun: Universal TUN/TAP device driver, 1.6
[    1.317127] tun: (C) 1999-2004 Max Krasnyansky <[email protected]>
[    1.317292] CAN device driver interface
[    1.318206] 2188000.ethernet supply phy not found, using dummy regulator
[    1.433600] pps pps0: new PPS source ptp0
[    1.479252] libphy: fec_enet_mii_bus: probed
[    1.479717] fec 2188000.ethernet eth0: registered PHC device 0
[    1.479905] PPP generic driver version 2.4.2
[    1.480091] PPP BSD Compression module registered
[    1.480094] PPP Deflate Compression module registered
[    1.480116] PPP MPPE Compression module registered
[    1.480121] NET: Registered protocol family 24
[    1.480194] usbcore: registered new interface driver asix
[    1.480249] usbcore: registered new interface driver ax88179_178a
[    1.480288] usbcore: registered new interface driver cdc_ether
[    1.480325] usbcore: registered new interface driver cdc_eem
[    1.480363] usbcore: registered new interface driver net1080
[    1.480401] usbcore: registered new interface driver cdc_subset
[    1.480437] usbcore: registered new interface driver zaurus
[    1.480514] usbcore: registered new interface driver cdc_ncm
[    1.480518] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.480521] ehci-mxc: Freescale On-Chip EHCI Host driver
[    1.480660] usbcore: registered new interface driver cdc_acm
[    1.480662] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.480719] usbcore: registered new interface driver usb-storage
[    1.480819] usbcore: registered new interface driver usbserial
[    1.480860] usbcore: registered new interface driver usbserial_generic
[    1.480894] usbserial: USB Serial support registered for generic
[    1.480929] usbcore: registered new interface driver ftdi_sio
[    1.480962] usbserial: USB Serial support registered for FTDI USB Serial Device
[    1.481002] usbcore: registered new interface driver option
[    1.481034] usbserial: USB Serial support registered for GSM modem (1-port)
[    1.481076] usbcore: registered new interface driver usb_ehset_test
[    1.481812] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[    1.489791] ci_hdrc ci_hdrc.1: doesn't support gadget
[    1.489809] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    1.489834] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[    1.503290] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    1.503459] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    1.503468] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    1.503474] usb usb1: Product: EHCI Host Controller
[    1.503479] usb usb1: Manufacturer: Linux 3.14.52-09424-g6fe6e7b-dirty ehci_hcd
[    1.503485] usb usb1: SerialNumber: ci_hdrc.1
[    1.504077] hub 1-0:1.0: USB hub found
[    1.504110] hub 1-0:1.0: 1 port detected
[    1.505006] mousedev: PS/2 mouse device common for all mice
[    1.505469] usbcore: registered new interface driver usbtouchscreen
[    1.505945] input: st1232-touchscreen as /devices/soc0/soc.0/2100000.aips-bus/21a8000.i2c/i2c-2/2-0055/input/input0
[    1.506776] snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
[    1.507057] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
[    1.507150] i2c /dev entries driver
[    1.508263] 2-003c supply DOVDD not found, using dummy regulator
[    1.508321] 2-003c supply DVDD not found, using dummy regulator
[    1.508357] 2-003c supply AVDD not found, using dummy regulator
[    1.663409] ata1: SATA link down (SStatus 0 SControl 300)
[    1.663449] ahci-imx 2200000.sata: no device found, disabling link.
[    1.663455] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[    1.698228] ov5640_read_reg:write reg error:reg=300a
[    1.698230] camera ov5640_mipi is not found
[    1.698986] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video16
[    1.699113] mxc_v4l2_output v4l2_out.23: V4L2 device registered as video17
[    1.699381] usbcore: registered new interface driver uvcvideo
[    1.699383] USB Video Class driver (1.1.1)
[    1.699628] [UDOO power-off] Probed LVDS power.
[    1.699709] [UDOO power-off] Probed LVDS backlight.
[    1.699777] [UDOO power-off] Probed UDOO Quad/Dual.
[    1.700170] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
[    1.700487] device-mapper: uevent: version 1.0.3
[    1.700808] device-mapper: ioctl: 4.27.0-ioctl (2013-10-30) initialised: [email protected]
[    1.701182] sdhci: Secure Digital Host Controller Interface driver
[    1.701184] sdhci: Copyright(c) Pierre Ossman
[    1.701187] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.706530] mmc0: no vqmmc regulator found
[    1.706536] mmc0: no vmmc regulator found
[    1.743251] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[    1.743904] Warning: No contiguous memory is reserverd for gpu.!
[    1.743904]  
[    1.743910] Warning: Will use default value(134217728) for the reserved memory!
[    1.743910]  
[    1.743915] Galcore version 5.0.11.41671
[    1.843372] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[    1.937342] mmc0: host does not support reading read-only switch. assuming write-enable.
[    1.955177] mmc0: new high speed SDHC card at address 0007
[    1.955877] mmcblk0: mmc0:0007 SD32G 29.0 GiB
[    1.990075]  mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
[    2.042141] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[    2.042150] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[    2.048796] hub 1-1:1.0: USB hub found
[    2.056750] hub 1-1:1.0: 4 ports detected
[    2.256969] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[    2.257492] mxc_vpu 2040000.vpu: VPU initialized
[    2.373516] usb 1-1.3: new high-speed USB device number 3 using ci_hdrc
[    2.503521] caam 2100000.caam: Instantiated RNG4 SH0
[    2.521267] usb 1-1.3: New USB device found, idVendor=148f, idProduct=5370
[    2.528169] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[    2.535534] usb 1-1.3: Product: 802.11 n WLAN
[    2.539901] usb 1-1.3: Manufacturer: Ralink
[    2.544107] usb 1-1.3: SerialNumber: 1.0
[    2.748725] caam 2100000.caam: Instantiated RNG4 SH1
[    2.753720] caam 2100000.caam: device ID = 0x0a160100 (Era 4)
[    2.759477] caam 2100000.caam: job rings = 2, qi = 0
[    2.826143] caam algorithms registered in /proc/crypto
[    2.834941] caam_jr 2101000.jr0: registering rng-caam
[    2.840811] snvs-secvio 20cc000.caam-snvs: can't get snvs clock
[    2.846782] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
[    2.855086] hidraw: raw HID events driver (C) Jiri Kosina
[    2.862822] usbcore: registered new interface driver usbhid
[    2.868446] usbhid: USB HID core driver
[    2.873031] ashmem: initialized
[    2.876387] logger: created 256K log 'log_main'
[    2.881078] logger: created 256K log 'log_events'
[    2.885964] logger: created 256K log 'log_radio'
[    2.890743] logger: created 256K log 'log_system'
[    2.896255] usbcore: registered new interface driver snd-usb-audio
[    2.903878] fsl-asrc 2034000.asrc: driver registered
[    2.973557] VT1613 SoC Audio Codec [ID = 5649 - 4123]
[    2.981651] imx-ac97-vt1613 sound.18: vt1613-hifi-analog <-> 2028000.ssi mapping ok
[    2.993550] imx-audio-hdmi sound-hdmi.19: hdmi-hifi <-> hdmi_audio.3 mapping ok
[    3.001688] NET: Registered protocol family 26
[    3.006175] u32 classifier
[    3.008890]     Actions configured
[    3.012300] Netfilter messages via NETLINK v0.30.
[    3.017093] nf_conntrack version 0.5.0 (16046 buckets, 64184 max)
[    3.023745] ctnetlink v0.93: registering with nfnetlink.
[    3.029601] xt_time: kernel timezone is -0000
[    3.034292] ip_tables: (C) 2000-2006 Netfilter Core Team
[    3.039768] arp_tables: (C) 2002 David S. Miller
[    3.044465] TCP: cubic registered
[    3.047789] Initializing XFRM netlink socket
[    3.052514] NET: Registered protocol family 10
[    3.057978] mip6: Mobile IPv6
[    3.060985] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    3.066610] sit: IPv6 over IPv4 tunneling driver
[    3.071846] NET: Registered protocol family 17
[    3.076344] NET: Registered protocol family 15
[    3.080797] can: controller area network core (rev 20120528 abi 9)
[    3.087051] NET: Registered protocol family 29
[    3.091505] can: raw protocol (rev 20120528)
[    3.095796] can: broadcast manager protocol (rev 20120528 t)
[    3.101469] can: netlink gateway (rev 20130117) max_hops=1
[    3.107118] 8021q: 802.1Q VLAN Support v1.8
[    3.111547] Key type dns_resolver registered
[    3.115991] Bluetooth: RFCOMM TTY layer initialized
[    3.120894] Bluetooth: RFCOMM socket layer initialized
[    3.126076] Bluetooth: RFCOMM ver 1.11
[    3.129925] usbcore: registered new interface driver btusb
[    3.135501] usbcore: registered new interface driver cdc_wdm
[    3.142719] ThumbEE CPU extension supported.
[    3.147741] usb_otg_vbus: disabling
[    3.151249] regulator-dummy: disabling
[    3.155558] file system registered
[    3.159742] using random self ethernet address
[    3.164238] using random host ethernet address
[    3.168764] Number of LUNs=8
[    3.171654] Mass Storage Function, version: 2009/09/11
[    3.176820] LUN: removable file: (no medium)
[    3.181319] android_usb gadget: android_usb ready
[    3.186276] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:07:33 UTC (453)
[    3.203341] ALSA device list:
[    3.206330]   #0: vt1613-audio
[    3.209404]   #1: imx-hdmi-soc
[    3.213045] Freeing unused kernel memory: 288K (c095a000 - c09a2000)
[    3.221809] init: init started!
[    3.226896] init: init second stage started!
[    3.231791] init: waitpid failed: No child processes
[    3.236964] init: property_set("ro.zygote", "zygote32") failed
[    3.243020] init: (Loading properties from /default.prop took 0.01s.)
[    3.251620] init: (Parsing /init.environ.rc took 0.00s.)
[    3.257357] init: (Parsing /init.usb.rc took 0.00s.)
[    3.263374] init: (Parsing init.freescale.usb.rc took 0.00s.)
[    3.269217] init: (Parsing init.freescale.i.MX6Q.rc took 0.00s.)
[    3.275383] init: (Parsing init.bluetooth.rc took 0.00s.)
[    3.280805] init: (Parsing /init.freescale.rc took 0.02s.)
[    3.286872] init: (Parsing /init.usb.configfs.rc took 0.00s.)
[    3.292724] init: (Parsing /init.zygote32.rc took 0.00s.)
[    3.298285] init: (Parsing /init.trace.rc took 0.00s.)
[    3.303477] init: (Parsing /init.rc took 0.05s.)
[    3.308291] init: Starting service 'ueventd'...
[    3.313405] init: Waiting for /dev/.coldboot_done...
[    3.315134] ueventd: ueventd started!
[    3.401670] uåÑ›Ù_œá«V“ú[    3.406169] init: write_file: Unable to open '/proc/sys/kernel/hung_task_timeout_secs': No such file or directory
[    3.416617] init: write_file: Unable to open '/proc/sys/kernel/sched_tunable_scaling': No such file or directory
[    3.426887] init: write_file: Unable to open '/proc/sys/kernel/sched_latency_ns': No such file or directory
[    3.436701] init: write_file: Unable to open '/proc/sys/kernel/sched_wakeup_granularity_ns': No such file or directory
[    3.447469] init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory
[    3.458259] init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
[    3.468081] init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
[    3.476668] init: Starting service 'watchdogd'...
[    3.482165] Console: switching to colour dummy device 80x30
[    3.489233] watchdogd: watchdogd started (interval 10, margin 20)!
[    3.512908] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: barrier=1
[    3.521369] fs_mgr: __mount(source=/dev/block/mmcblk0p5,target=/system,type=ext4)=0
[    3.530216] EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option
[    3.544467] JBD2: recovery failed
[    3.547800] EXT4-fs (mmcblk0p4): error loading journal
[    3.553173] fs_mgr: __mount(source=/dev/block/mmcblk0p4,target=/data,type=ext4)=-1
[    3.562594] fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk0p4 for mount /data type ext4 )
[    3.574705] EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option
[    3.588424] JBD2: recovery failed
[    3.591752] EXT4-fs (mmcblk0p6): error loading journal
[    3.597132] fs_mgr: __mount(source=/dev/block/mmcblk0p6,target=/cache,type=ext4)=-1
[    3.607110] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p6 at /cache options: nomblk_io_submit error: Invalid argument
[    3.624964] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
[    3.633095] fs_mgr: __mount(source=/dev/block/mmcblk0p7,target=/device,type=ext4)=0
[    3.640885] init: fs_mgr_mount_all returned an error
[    3.646115] init: fs_mgr_mount_all returned unexpected error 255
[    3.655366] init: Starting service 'logd'...
[    3.854781] random: mkswap urandom read with 30 bits of entropy available
[    3.864217] Adding 307196k swap on /dev/block/zram0.  Priority:-1 extents:1 across:307196k SS
[    3.894278] init: (Loading properties from /system/build.prop took 0.02s.)
[    3.901321] init: (Loading properties from /vendor/build.prop took 0.00s.)
[    3.908696] init: (Loading properties from /factory/factory.prop took 0.00s.)
[    3.918508] init: Starting service 'vold'...
[    3.922730] logd.auditd: start
[    3.922767] logd.klogd: 3919536666
[    3.930236] init: Not bootcharting.
[    3.935322] init: Failed to reload policy
[    3.939661] init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...
[    3.971229] init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 184) exited with status 0
[    3.980136] init: (Loading properties from /data/local.prop took 0.00s.)
[    3.986993] init: Starting service 'logd-reinit'...
[    3.995242] init: Starting service 'healthd'...
[    4.000308] init: Starting service 'console'...
[    4.003215] binder: 193:193 transaction failed 29189, size 0-0
At¨  >ù›[    4.012601] init: Starting service 'servicemanager'...
[    4.018383] init: Starting service 'surfaceflinger'...
[    4.030002] init: Starting service 'daemonsu'...
[    4.030317] logd.daemon: reinit
[    4.038689] init: Service 'logd-reinit' (pid 190) exited with status 0
[    4.046153] init: Starting service 'exec 1 (/system/bin/fakerclocal)'...
[    4.091215] warning: `daemonsu' uses 32-bit capabilities (legacy support in use)
root@udoo_6dq:/ # [    4.101010] init: Service 'daemonsu' (pid 208) exited with status 0
[    4.248258] init: Service 'exec 1 (/system/bin/fakerclocal)' (pid 212) exited with status 0
[    4.283738] cfg80211: Calling CRDA to update world regulatory domain
[    4.290284] cfg80211: World regulatory domain updated:
[    4.295496] cfg80211:  DFS Master region: unset
[    4.299862] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[    4.309900] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[    4.317950] cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    4.327389] cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[    4.335434] cfg80211:   (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    4.345010] cfg80211:   (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[    4.354568] cfg80211:   (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[    4.362680] cfg80211:   (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[    4.370711] cfg80211:   (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[    4.416839] init: property_set("ro.ril.wake_lock_timeout", "300") failed
[    4.424510] init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
[    4.433856] init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
[    4.444211] init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
[    4.455180] init: Starting service 'disableadk'...
[    4.492947] init: Service 'disableadk' (pid 248) exited with status 0
[    5.004352] healthd: No charger supplies found
[    5.004381] healthd: No battery devices found
[    5.256877] init: Starting service 'bootanim'...
[    9.280707] random: nonblocking pool is initialized

ラベル(5)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,305件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Julian

what bsp used in the case, one can try with nxp android releases described on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

In general for reliable reboot it is necessary to shortly remove power fom all board

using pmic pwron signal as in spf-27392 i.MX6Q Sabre SD schematic p.21.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,305件の閲覧回数
julianmp
Contributor II

I have the same issue if a shutdown or unplugged directly, this is a udoo board, and if I flash the sdcard with his android image doesn't occur, but if i compile their android i have this issue

0 件の賞賛
返信