Android 6.0 CTS security item test fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 6.0 CTS security item test fail

2,167 Views
felixhsu
Contributor III

Hi All

The customer run  Android 6.0 CTS will happened security item fail, the fail item as below, 

fail.png

Can you provide patch file or any suggest?

Thanks.

Labels (2)
0 Kudos
Reply
3 Replies

1,960 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Which i.MX SOC is using your customer?

Best Regards,

Diego

0 Kudos
Reply

1,960 Views
felixhsu
Contributor III

Hi Diego

Use the i.MX6Quad SOC.

Thanks.

0 Kudos
Reply

1,960 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Do you happen to know which Android 6.0 release is your customer using? and also the CTS version?

 

I believe that upgrading to android O8.0.0_1.0.0_GA may help on this case, looking at the CTS 8.0_r4 test report for i.MX6Q SabreSD the following tests are marked as passed which fails in your customer side.

Hope this can help you.

Best Regards,

Diego.

0 Kudos
Reply