Android 6.0.1 File Transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 6.0.1 File Transfer

2,884件の閲覧回数
jian_jiang
NXP Employee
NXP Employee

Hi,

It seems that Windows7 cannot detect i.MX6Q(and i.MX6DL) SDB when the board is in file transfer mode (MTP) in Android 6.0.1_2.0.0.

But the photo transfer mode (PTP) works fine, so I always copy files into /sdcard/DCIM folder and transfer to other folders in the console.

The Android KK4.4.2 works fine in MTP.

So any ideas to improve the MTP mode in Android 6.0.1?

All the best

Kane

ラベル(2)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,620件の閲覧回数
ferenwer
Contributor I

Transfer data from phone to computer, you can try some data backup softwares, and I think it can be easier with an android assistant app, you can save a lot of time to transfer or backup text messages, contacts, photos, and other media files like videos, music files.

0 件の賞賛
返信

2,620件の閲覧回数
jian_jiang
NXP Employee
NXP Employee

Hi feren,

Thanks for your comment!

Yes, it is worth to try some apps.

0 件の賞賛
返信

2,620件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  From "Android_Frequently_Asked_Questions.pdf" :
"In the Windows® 7 OS, in theory MTP can work together with ADB, but it is
also found that some hosts with the Windows 7 OS fail to support it."

  Please check ADB configuration.

Regards,

Yuri.

0 件の賞賛
返信

2,620件の閲覧回数
jian_jiang
NXP Employee
NXP Employee

Hi, Yuri

Thanks for your reply.

When I enabled the "USB debugging" in "Developer options", the storage device of the board did not appear in "Computer". But there is an icon for ejecting board in the lower right corner and a unknown MTP device in "Device Manager".

When I disabled the "USB debugging" in "Developer options", the storage device of the board also did not appear in "Computer". And there is no icon for ejecting board in the lower right corner. With a unknown SABRESD-MX6DQ device in "Device Manager".

All the best

Kane

0 件の賞賛
返信