Analog PLL Duplicate Registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Analog PLL Duplicate Registers

1,289件の閲覧回数
dougbailey
Contributor III

In the iMX6DL reference manual, there are a series of CCM configuration registers for the analog PLL's where the description includes something like: 

Address: 20C_8000h base + 0h offset + (4d × i), where i=0d to 3d

I am confused as to what 'i' actually represents.

Are these just duplicate registers i.e. the same register duplicates 4 times?

Is there some intrinsic meaning in the i and that manipulating 0x20c8000 is different from manipulating 0x20c8004?

 

From all I can tell, these are just duplicates.  Can someone tell me otherwise? 

Regards

Doug Bailey 

ラベル(1)
0 件の賞賛
返信
1 返信

1,171件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Doug

please refer to sect.18.7 CCM Analog Memory Map/Register Definition i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

Registers _SET,_CLR,_TOG used to set, clear and toggle selected bits.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信