[Android 5.0.2] The RTC function is fail.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[Android 5.0.2] The RTC function is fail.

跳至解决方案
4,442 次查看
charleshuang
Senior Contributor II

Hi Freescale

We test the RTC function in Android 5.0.2 version on Demo board.

We tried to change the time.

After system reboot,the time is default value.

The RTC function is fail in Android 5.0.2.

But we try to send command,the RTC function is pass.

example:

# busybox date 2015.10.16-10:41:26

# busybox hwclock -w

# busybox hwclock

Do you have any advice?

标签 (4)
0 项奖励
回复
1 解答
4,045 次查看
kamilbystryk
Contributor III

Charles, did You found solution for RTC settings problem? I see it marked as resolved on.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,045 次查看
eric-system
Contributor I

Hi All, 

I also met the problem which RTC seeing failed in Android 5.1, does anyone can tell me solution for this issue

Thanks a lot.

Eric

0 项奖励
回复
4,045 次查看
richardmlewis
Contributor I
0 项奖励
回复
4,045 次查看
charleshuang
Senior Contributor II

Hi Kamil Bystryk

I already found the solution and fixed the issue for RTC settting.  Thanks

0 项奖励
回复
4,045 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi charleshuang,

Would you be nice enough to share your solution? It would be very appreciated and helpful.

Best Regards,

Alejandro

0 项奖励
回复
4,045 次查看
kamilbystryk
Contributor III

OK, but - can You help me with this problem? I try to resolve the same error. Thanks.

0 项奖励
回复
4,046 次查看
kamilbystryk
Contributor III

Charles, did You found solution for RTC settings problem? I see it marked as resolved on.

0 项奖励
回复