Some feedback to i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 3, 07/2015

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some feedback to i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 3, 07/2015

1,775 Views
martin_maurer
Contributor III


Hello,

[Info/pages updated from rev. 1 to rev. 3, 07/2015]

here some feedback to "i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 3, 07/2015".

1) According to page 507 PLL5 seem to go from 650MHz to 1300MHz.

But page 796 list 630MHz as one and only frequency. Cut&Paste error from PLL4?

2) Is 132MHz as default frequency correct for IPU2_DI0_CLK_ROOT? All other IPUx_DIy_CLK_ROOT show 180MHz...

(Page 808)

3) Page 859 shows "Selector for ldb_di1 clock multiplexer" even for "11–9 ldb_di0_clk_sel".

4) Page 1625: "Input video Vertical active pixel region width. Number of Vertical active lines [0...4095]."

But field has only 8 bits, so max 255?

5) Page 2892: IPU_DP_COM_CONF_SYNC Register address 0x1F40000. Correct? Same for SRM entries

and all following entries up to following page and register IPU_DP_CSC_ASYNC1_1?

(to page 2893 and 2894)

6) Page 3251: Bit 18: "Post-Processing Task color conversion RGB-->YUV enable. This bit enables YUV-->RGB."

Must be "RGB-->YUV" at end of sentence?

Best regards,

Martin

Labels (2)
0 Kudos
Reply
3 Replies

1,466 Views
b36401
NXP Employee
NXP Employee

The points 1,2,3,6 you noted seem to be typos.

As for page 1625 (and 1622 as well) please note that actually there are HDMI_FC_INVACTIV0+HDMI_FC_INVACTIV1 pair 8bit registers that provides whole 13bit value.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,466 Views
martin_maurer
Contributor III

Hello Victor,

two new things:

1) Just found another small typo: Search for "resister" (occures multiple times, in titles and even later in the text), in my opinion shall be "register".

2) I think a clarification is needed for TEMPMON:

"62.3.1 Tempsensor Control Register 0 (TEMPMON_TEMPSENSE0n)"

-> There is a "n" inside the register name.

"Address: 20C_8000h base + 180h offset + (4d × i), where i=0d to 3d"

-> Address calculation shows "i" goes from 0 to 3.

=> Do we have more than 1 temperature sensor? One for each core?

But OCOTP_ANA1 is only available 1 times, so common for all temperature sensors?

Any updates on the other topics?

Best regards,

Martin

0 Kudos
Reply

1,466 Views
martin_maurer
Contributor III

As for page 1625 (and 1622 as well) please note that actually there are HDMI_FC_INVACTIV0+HDMI_FC_INVACTIV1 pair 8bit registers that provides whole 13bit value.

Perhaps the "other" register can be added as in description of register?

0 Kudos
Reply