[Android 5.0.2] The RTC function is fail.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Android 5.0.2] The RTC function is fail.

ソリューションへジャンプ
4,445件の閲覧回数
charleshuang
Senior Contributor II

Hi Freescale

We test the RTC function in Android 5.0.2 version on Demo board.

We tried to change the time.

After system reboot,the time is default value.

The RTC function is fail in Android 5.0.2.

But we try to send command,the RTC function is pass.

example:

# busybox date 2015.10.16-10:41:26

# busybox hwclock -w

# busybox hwclock

Do you have any advice?

ラベル(4)
0 件の賞賛
返信
1 解決策
4,048件の閲覧回数
kamilbystryk
Contributor III

Charles, did You found solution for RTC settings problem? I see it marked as resolved on.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,048件の閲覧回数
eric-system
Contributor I

Hi All, 

I also met the problem which RTC seeing failed in Android 5.1, does anyone can tell me solution for this issue

Thanks a lot.

Eric

0 件の賞賛
返信
4,048件の閲覧回数
richardmlewis
Contributor I
0 件の賞賛
返信
4,048件の閲覧回数
charleshuang
Senior Contributor II

Hi Kamil Bystryk

I already found the solution and fixed the issue for RTC settting.  Thanks

0 件の賞賛
返信
4,048件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi charleshuang,

Would you be nice enough to share your solution? It would be very appreciated and helpful.

Best Regards,

Alejandro

0 件の賞賛
返信
4,048件の閲覧回数
kamilbystryk
Contributor III

OK, but - can You help me with this problem? I try to resolve the same error. Thanks.

0 件の賞賛
返信
4,049件の閲覧回数
kamilbystryk
Contributor III

Charles, did You found solution for RTC settings problem? I see it marked as resolved on.

0 件の賞賛
返信