Android 11 kernel booting issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 11 kernel booting issue

4,768 Views
siva172902
Contributor I

Hi,

We are doing android porting for verdin-imx8mp board.Took the android 11 OS for IMX8MP which is provided by NXP & modified the u-boot & kernel code w.r.t to the verdin development board.We are able to build the android os with the verdin board changes & able to generate images.

We got struck in flashing the android image on verdin-imax8mp board. Can you please guide me the flashing mechanism for verdin-imx8mp board?

Thanks & Regards,

Siva Sankar Reddy

0 Kudos
Reply
5 Replies

4,747 Views
siva172902
Contributor I

Hi,

We are doing android porting for verdin-imx8mp board.Took the android 11 OS for IMX8MP which is provided by NXP & modified the u-boot & kernel code w.r.t to the verdin development board.We are able to build the android os with the verdin board changes & able to generate images.

Flashed all the android images, u-boot is loading but not able to load kernel.It got struck in starting kernel....
Please find the attached log.

Thanks & Regards,

Siva Sankar Reddy

0 Kudos
Reply

4,707 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @siva172902,

I hope you are doing well.
 
Kindly confirm the procedure you are following and the environment variable settings as per mentioned in section 5.4 Booting from the AQSG Android ™ Quick Start Guide.pdf of Android 11.
 
One can download the document from the link below.
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply

4,702 Views
siva172902
Contributor I

Hi Dhruv,

 

I am following the same for environmental setup for booting.

 

Thanks & Regards,

Siva.

0 Kudos
Reply

4,661 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @siva172902,

I hope you are doing well
 
My apology for the delayed response.
 
Kindly check the Kernel command line (bootargs) is set as per your board.
One can reference the section 6.2.2 Kernel command line (bootargs) from the Android ™ User's Guide.
If it does not solve the issue, kindly share the values of your Uboot environment variables using the 'printenv' command for further debugging the issue.
 
Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply

4,753 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @siva172902,

I hope you are doing well
 
One can flash the binary into the EMMC using the UUU tool.
Please refer to section 5.3 Flashing board images from the ANDROID_QUICK_START_GUIDE.pdf
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply