Adding apt-get to fsl-image-gui 3.10.17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding apt-get to fsl-image-gui 3.10.17

1,085 Views
ScottKerstein
Contributor III

Hello,

apt-get command isn't available in the fsl-image-gui BSP I just compiled for SABRE-SDP using kernel 3.10.17.  What is the method to install it?  Do I need to add a recipe?

Thanks in advance,

Scott

Labels (3)
0 Kudos
Reply
1 Reply

734 Views
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

Re: Yocto with a package manager (ex: apt-get)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply