LVDS issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS issue

2,584 Views
lifusong
Contributor IV

dear sir.

    our lvds can who something.but ,have some problem,please see below pic.

how to fix this.

our lvds work on 800x480  18bit ,boot args is  video=mxcfb0:dev=ldb,if=RGB666,fbpix=RGB24 vmalloc=400M,

and use if=rgb24,this image is more worse.

pastedImage_0.png

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

2,154 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

for 800x480 lvds settings one can look at nitrogen board

Universal Boot Loader general discussion ()

[PATCH 17/32] nitrogen6x: display: add wvga-lvds panel

Theory&Example :

AN3974 Different Display Configurations on i.MX35 Linux PDK

how to support WSVGA output in imx6sdq

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,154 Views
lifusong
Contributor IV

our board is mx6q,and android version is 4.4.3_r1.  kernel 3.10.53  u-boot 2014.04

below is the u-boot seting.

static struct display_info_t const displays[] = {{

  .bus = -1,

  .addr = 0,

  .pixfmt = IPU_PIX_FMT_RGB666,

  .detect = NULL,

  .enable = NULL,

  .mode = {

  .name           = "Hannstar-XGA",

  .refresh        = 60,

  .xres           = 800,//1024,

  .yres           = 480,//768,

  .pixclock       = 19531,//15385,

  .left_margin    = 160,//220,

  .right_margin   = 160,//40,

  .upper_margin   = 18,//21,

  .lower_margin   = 18,//7,

  .hsync_len      = 60,

  .vsync_len      = 10,

  .sync           = FB_SYNC_EXT,

  .vmode          = FB_VMODE_NONINTERLACED

} }

below is the kernel device tree seting

lvds-channel@0 {
crtc = "ipu2-di0";
status = "okay";
fsl,data-mapping = "spwg";
fsl,data-width = <18>;

display-timings {
native-mode = <&timing0>;
timing0: hsd100pxn1 {
clock-frequency = <65000000>;
hactive = <800>;
vactive = <480>;
hback-porch = <160>;
hfront-porch = <160>;
vback-porch = <18>;
vfront-porch = <18>;
hsync-len = <60>;
vsync-len = <10>;
};
};
};
0 Kudos
Reply

2,154 Views
lifusong
Contributor IV

Dear sir.

   in that link.Universal Boot Loader general discussion ()

what is the base version?

I can't found the match line in u-boot 2014.04

0 Kudos
Reply