Adding apt-get to fsl-image-gui 3.10.17

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding apt-get to fsl-image-gui 3.10.17

1,088件の閲覧回数
ScottKerstein
Contributor III

Hello,

apt-get command isn't available in the fsl-image-gui BSP I just compiled for SABRE-SDP using kernel 3.10.17.  What is the method to install it?  Do I need to add a recipe?

Thanks in advance,

Scott

ラベル(3)
0 件の賞賛
返信
1 返信

737件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I hope the following helps.

Re: Yocto with a package manager (ex: apt-get)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信