Adding 2nd Ethernet interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding 2nd Ethernet interface

3,543件の閲覧回数
Riba
Contributor I

We are trying to add 2nd Ethernet MAC interface to Toradex Verdin iMX8MP. Our custom carrier board has only one External Ethernet port (ETH_1) , and we are trying to configure 2nd ethernet controller (ETH_2). Our device-tree for fec node:

here is fec node:
/* Verdin ETH_2_RGMII */
&fec {
fsl,magic-packet;
//phy-handle = <&ethphy1>;
phy-mode = "rgmii-id";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pinctrl_fec>;
pinctrl-1 = <&pinctrl_fec_sleep>;
phy-supply = <&reg_ext_rgmii>;

mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy1: ethernet-phy@Addr {
compatible = "ethernet-phy-ieee802.3-c22";
interrupt-parent = <&gpio4>;
interrupts = <18 IRQ_TYPE_LEVEL_LOW>;
phy-is-integrated;
micrel,led-mode = <0>;
reg = <Addr>;
};
};

we are getting following error:

[ 1.965324] 002: fec 30be0000.ethernet eth0: no PHY, assuming direct connection to switch mdio_bus_id = 303085963
[ 1.965345] 002: libphy: PHY fixed-0:00 not found
[ 1.965349] 002: fec 30be0000.ethernet eth0: could not attach to PHY

};

We are using linux BSP: Linux version 5.4.129-rt61-5.4.0-devel+git.022cb949c6ec 

Has anyone seen this issue before? How have you resolved it? 

Thanks

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,517件の閲覧回数
Riba
Contributor I

Thanks JoanXie for your response. Could you kindly look at into following device-tree changes to configure 2nd Ethernet on imx8mp as a MAC to another MAC interface.

&fec {
fsl,magic-packet;
// phy-mode = "rgmii-id";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pinctrl_fec>;
pinctrl-1 = <&pinctrl_fec_sleep>;

fixed-link {
speed = <1000>;
full-duplex;
pause;
};

mdio {
#address-cells = <1>;
#size-cells = <0>;
};
};

Any input greatly appreciated.

Thanks

 

0 件の賞賛
返信

3,533件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

this is not nxp imx8mp board, I suggest that you can contact the third party company to support this, for nxp bsp, supports second ethernet port in the dts as default, maybe you can refer to that

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.d...

and in the dtsi file define as below

ehernet0 = &fec;
ethernet1 = &eqos;

 

0 件の賞賛
返信

3,509件の閲覧回数
Riba
Contributor I

Thanks for your reply. Yes, we resolved this issue, no longer help needed.

0 件の賞賛
返信

3,330件の閲覧回数
Samhitha_Kashyap
Contributor III

Hello Riba,

We are facing a similar issue, can you please share the changes in the device tree, that was required to configure the second ethernet interface.

Thanks & Regards,

Samhitha

0 件の賞賛
返信

3,322件の閲覧回数
Riba
Contributor I

Hi Samhitha:

We modified device-tree per below, we are successfully communicating with 2nd Ethernet configured as MAC interface:

/* Verdin ETH_2_RGMII */
&fec {
fsl,magic-packet;
phy-mode = "rgmii-id";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&pinctrl_fec>;
pinctrl-1 = <&pinctrl_fec_sleep>;
//phy-supply = <&reg_module_eth2phy>;
status = "okay";

fixed-link {
speed = <1000>;
full-duplex;
pause;
};
mdio {
#address-cells = <1>;
#size-cells = <0>;
};
};

Best of luck.

0 件の賞賛
返信

3,311件の閲覧回数
Samhitha_Kashyap
Contributor III

Hi Riba,

Thanks for the response and sharing the device tree changes.

Best Regards,

Samhitha Kashyap

0 件の賞賛
返信