Add CAN Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,742件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

I am working on IMX8QM with Android 9. Currently, I am using imx-p9.0.0_2.1.1-auto-ga source. I needs to add CONFIG_CAN_FLEXCAN. But, I am unable to enable.

by using make menuconfig,

 

I got depends on  (ARM || ARM64 || PPC) - I don't how to add this dependency,

   Depends on: NET [=y] && CAN [=y] && CAN_DEV [=y] && (ARM || ARM64 || PPC) 

If I check ARM64,

   CONFIG_ARCH_MXC_ARM64 - CLKSRC_MMIO -etc,

 

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 解決策
3,539件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

As my understanding, you do not need to enable any module. Just is saying that the module could work for architectures ARM, ARM64, and Power PC. This is similar when you are initializing the toolchain, you write the macro ARCH=arm, or ARCH=arm64. 

 Best regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,539件の閲覧回数
vinothkumars
Senior Contributor IV

Will you please, provide the sample dotconfig files (included flex can dependency).

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
3,539件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

The (ARM || ARM64 || PPC) is saying that it is supported by the architecture ARM, ARM64 or Power PC. In this case, it is the Architecture ARM64.

Best regards,

Diego.

0 件の賞賛
返信
3,539件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you Diego,

If it possible, Will you please guide me, how to enable ARM64 in Kernel config.

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
3,540件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

As my understanding, you do not need to enable any module. Just is saying that the module could work for architectures ARM, ARM64, and Power PC. This is similar when you are initializing the toolchain, you write the macro ARCH=arm, or ARCH=arm64. 

 Best regards,

Diego.

0 件の賞賛
返信
3,539件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you Diego for your reply.

Thanks @ Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信