Adc values read from boot loader in IMx6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adc values read from boot loader in IMx6UL

884件の閲覧回数
sankarsalla
Contributor II

Hi All,

In my project need to read adc values from boot loader.

Adc values are read from root file system happens through sysfs entries and properly working.

Same thing i need to read from boot loader,i have checked in boot loader source adc driver is not there.

can you help me how to port adc driver in boot loader.

Thanks & Regards,

Sankar.      

ラベル(1)
0 件の賞賛
返信
1 返信

807件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sankar

for baremetal adc examples one can look at freertos:

Board Support Packages (7)
SDK2.2_iMX6UL_WIN(REV SDK2.2)

i.MX 6UltraLite Applications Processor | Single Arm® Cortex®-A7 @ 696 MHz |NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信