Adc values read from boot loader in IMx6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adc values read from boot loader in IMx6UL

926 Views
sankarsalla
Contributor II

Hi All,

In my project need to read adc values from boot loader.

Adc values are read from root file system happens through sysfs entries and properly working.

Same thing i need to read from boot loader,i have checked in boot loader source adc driver is not there.

can you help me how to port adc driver in boot loader.

Thanks & Regards,

Sankar.      

Labels (1)
0 Kudos
Reply
1 Reply

849 Views
igorpadykov
NXP Employee
NXP Employee

Hi sankar

for baremetal adc examples one can look at freertos:

Board Support Packages (7)
SDK2.2_iMX6UL_WIN(REV SDK2.2)

i.MX 6UltraLite Applications Processor | Single Arm® Cortex®-A7 @ 696 MHz |NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply