Accessing Parallel Nor flash in Kernel Command Line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing Parallel Nor flash in Kernel Command Line

ソリューションへジャンプ
2,248件の閲覧回数
nishad_kamdar
Contributor IV

Hi ,

I have a custom iMX6q board in which i have a parallel nor flash connected to the Processor.

I am able to read and write to it in u-boot using the "md" command however i am not able to do it in

Kernel command line after my linux boots.

Can anyone tell me how i can read and write to the Nor flash.

regards,

nishad

ラベル(1)
0 件の賞賛
返信
1 解決策
2,125件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may use "memtool" utility in /unit/tests directory.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,126件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may use "memtool" utility in /unit/tests directory.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信