Accessing Parallel Nor flash in Kernel Command Line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Accessing Parallel Nor flash in Kernel Command Line

跳至解决方案
2,189 次查看
nishad_kamdar
Contributor IV

Hi ,

I have a custom iMX6q board in which i have a parallel nor flash connected to the Processor.

I am able to read and write to it in u-boot using the "md" command however i am not able to do it in

Kernel command line after my linux boots.

Can anyone tell me how i can read and write to the Nor flash.

regards,

nishad

标签 (1)
0 项奖励
回复
1 解答
2,066 次查看
Yuri
NXP Employee
NXP Employee

You may use "memtool" utility in /unit/tests directory.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,067 次查看
Yuri
NXP Employee
NXP Employee

You may use "memtool" utility in /unit/tests directory.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复