About the u-boot-imx*_sd_optee.imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the u-boot-imx*_sd_optee.imx

Jump to solution
488 Views
liuxing
Contributor II

Hi All,

  I want to port optee os on imx6q SOC platform.I find some porting info in IMX_PORTING_GUIDE.pdf(UG10165)

5.3 OP-TEE booting flow
Booting flow on i.MX 6 and i.MX 7 (Arm V7):
Files and binaries required in the boot partition:
• u-boot-imx*_sd_optee.imx: U-Boot binary specific to boot OP-TEE. Only booting from the SD card is
supported for OP-TEE.
• uTee-*: Self-extracting image containing the OP-TEE binary.

 

I want to know how to generate the u-boot-imx*_sd_optee.imx image,and which uboot config file I can use.

Tags (1)
0 Kudos
Reply
1 Solution
462 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @liuxing 

You can use the one - mx6qpsabresd_optee_defconfig

Send you more information in system email.

 

Regards

Harvey

View solution in original post

0 Kudos
Reply
1 Reply
463 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @liuxing 

You can use the one - mx6qpsabresd_optee_defconfig

Send you more information in system email.

 

Regards

Harvey

0 Kudos
Reply