About the u-boot-imx*_sd_optee.imx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the u-boot-imx*_sd_optee.imx

跳至解决方案
481 次查看
liuxing
Contributor II

Hi All,

  I want to port optee os on imx6q SOC platform.I find some porting info in IMX_PORTING_GUIDE.pdf(UG10165)

5.3 OP-TEE booting flow
Booting flow on i.MX 6 and i.MX 7 (Arm V7):
Files and binaries required in the boot partition:
• u-boot-imx*_sd_optee.imx: U-Boot binary specific to boot OP-TEE. Only booting from the SD card is
supported for OP-TEE.
• uTee-*: Self-extracting image containing the OP-TEE binary.

 

I want to know how to generate the u-boot-imx*_sd_optee.imx image,and which uboot config file I can use.

标记 (1)
0 项奖励
回复
1 解答
455 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @liuxing 

You can use the one - mx6qpsabresd_optee_defconfig

Send you more information in system email.

 

Regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
1 回复
456 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @liuxing 

You can use the one - mx6qpsabresd_optee_defconfig

Send you more information in system email.

 

Regards

Harvey

0 项奖励
回复