About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the Wake on LAN sample source code for MX6DL-SABRE-SDP Linux BSP

ソリューションへジャンプ
2,880件の閲覧回数
yuuki
Senior Contributor II

Dear all,


Our customer wants to make a system using i.MX6Solo and PF0100.
They are going to wake-up a system by an Ethernet.


I have the following several questions.

1)
According to section "23.5.7.1 Sleep mode"(P.1132) of a reference manual, the following is explained.
"In addition, when the processor is in Stop mode, Sleep mode is entered, without affecting the ENETn_ECR register bits.

When a processor is Standby or Deep Sleep mode, can MAC enter a Sleep mode?


2)
They use LinuxBSP.
Is there a sample cord for a system to be waked-up by a Magic packet of Ethernet?


Best Regards,
Yuuki

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,572件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

official linux BSP does not support wake on lan, however

there is Community patch below

Wake on lan in mx6 sabresd board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

official linux BSP does not support wake on lan, however

there is Community patch below

Wake on lan in mx6 sabresd board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信