Question, i.MX28 EMI/ additive latency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question, i.MX28 EMI/ additive latency

跳至解决方案
1,790 次查看
Aemj
Contributor IV

Dear team,

I would like to ask about i.MCX28 EMI/ additive latency.

In i.MX28 reference manual, it is said the EMI does not support ‘additive latency’.

In my understanding,

If one needs to add additive latency, then one has to add the additive latency into CASLAT and also WRLAT parameter.

Am I correct?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 解答
1,678 次查看
Yuri
NXP Employee
NXP Employee

   Additive latency  (in the JEDEC Specification) allows a read or write command to be issued
immediately following the active command. In this sense we cannot  "add the additive latency"

for i.MX28.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,679 次查看
Yuri
NXP Employee
NXP Employee

   Additive latency  (in the JEDEC Specification) allows a read or write command to be issued
immediately following the active command. In this sense we cannot  "add the additive latency"

for i.MX28.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复