About the LICELL PIN when not using RTC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the LICELL PIN when not using RTC

跳至解决方案
2,217 次查看
george
Senior Contributor II

Dear all,

When using i.MX6 and MMPF0100 together like i.MX6-SDP and the RTC function is unnecessary, should the LICELL pin of PMIC be open?

Or is it necessary to tie to the power supply of suitable voltage?

Best Regards,

George

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,064 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

when not used, it should be bypassed with 0.1uF as suggests

AN4717 AN4717, Schematic Guidelines for the MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,065 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

when not used, it should be bypassed with 0.1uF as suggests

AN4717 AN4717, Schematic Guidelines for the MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,064 次查看
george
Senior Contributor II

Dear igor,

Thanks.

0 项奖励
回复