About the LICELL PIN when not using RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the LICELL PIN when not using RTC

ソリューションへジャンプ
2,219件の閲覧回数
george
Senior Contributor II

Dear all,

When using i.MX6 and MMPF0100 together like i.MX6-SDP and the RTC function is unnecessary, should the LICELL pin of PMIC be open?

Or is it necessary to tie to the power supply of suitable voltage?

Best Regards,

George

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,066件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

when not used, it should be bypassed with 0.1uF as suggests

AN4717 AN4717, Schematic Guidelines for the MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,067件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

when not used, it should be bypassed with 0.1uF as suggests

AN4717 AN4717, Schematic Guidelines for the MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,066件の閲覧回数
george
Senior Contributor II

Dear igor,

Thanks.

0 件の賞賛
返信