About the GPU driver patch for iMX6 on Freescale git servier

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the GPU driver patch for iMX6 on Freescale git servier

跳至解决方案
3,296 次查看
brianwu
Contributor III

Hi community,

I found these is a new 3.10.31 kernel branch on the Freescale Git server.

I compare the 3.10.17 and 3.10.31 kernel patches about the gpu driver:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.31_1.1.0_alpha&qt=grep&q...

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.17_1.0.0_ga&qt=grep&q=gp...

And I found there are some new patches in the 3.10.31 kernel.

Do you suggest to implement these new patches in the 3.10.17 kernel?

BR

Brian

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,241 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Brian,

The one that you should use is the

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.17_1.0.0_ga&qt=grep&q=gp...

Because this one is the tested release of the driver.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,242 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Brian,

The one that you should use is the

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.17_1.0.0_ga&qt=grep&q=gp...

Because this one is the tested release of the driver.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复