About supporting the DDR3L in i.MX6SL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About supporting the DDR3L in i.MX6SL

ソリューションへジャンプ
1,426件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about supporting the DDR3L in i.MX6SL

I referred below community.

i.MX6SL NVCC_DRAM for DDR3L.

> DDR3L support is notD yet for i.MX6 SL.

Is it possible to use the DDR3L in i.MX6SL?

And, have freescale finished the fully validation / characterization for DDR3L?

Best Regards,

Keita

ラベル(1)
0 件の賞賛
返信
1 解決策
1,211件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

  Alas, the situation is still the same, as mentioned in i.MX6SL NVCC_DRAM for DDR3L.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,212件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

  Alas, the situation is still the same, as mentioned in i.MX6SL NVCC_DRAM for DDR3L.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信