About supporting the DDR3L in i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About supporting the DDR3L in i.MX6SL

Jump to solution
1,102 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about supporting the DDR3L in i.MX6SL

I referred below community.

i.MX6SL NVCC_DRAM for DDR3L.

> DDR3L support is notD yet for i.MX6 SL.

Is it possible to use the DDR3L in i.MX6SL?

And, have freescale finished the fully validation / characterization for DDR3L?

Best Regards,

Keita

Labels (1)
0 Kudos
Reply
1 Solution
887 Views
Yuri
NXP Employee
NXP Employee

Hi,

  Alas, the situation is still the same, as mentioned in i.MX6SL NVCC_DRAM for DDR3L.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
888 Views
Yuri
NXP Employee
NXP Employee

Hi,

  Alas, the situation is still the same, as mentioned in i.MX6SL NVCC_DRAM for DDR3L.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply