About selects between two possible sources for SDMA_EVENT in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About selects between two possible sources for SDMA_EVENT in i.MX6DQ.

跳至解决方案
1,031 次查看
keitanagashima
Senior Contributor I

Dear all,

Hello. I have a question about selection between two possible sources for SDMA_EVENT in i.MX6DQ.

BSP: L3.0.35_4.1.0

Refer to "IOMUXC_GPR0 field descriptions" in MCIMX6DQRMM(Rev.2).

DMAREQ_MUX_SEL0 bit of register IOMUXC_GPR0, let us to Selects between two possible sources for SDMA_EVENT[2]:

0 ipu1.ipu_sdma_event  (we think it is related with ipu1)

1 hdmi_tx.hdmi_tx_ophydtb[0] (we think it is related with hdmi tx audio)

[Question]

Is it OK to use both ipu1 and hdmi tx audio?

If it is not OK and we want to use both ipu1 and hdmi tx audio at the same time, could you help us to provide the method?

Best Regards,

Keita

标签 (3)
0 项奖励
回复
1 解答
968 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  as for  "Is it OK to use both ipu1 and hdmi tx audio?" - BSP does not

use SDMA for IPU operations, therefore it is possible both modules at the same

time.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
969 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  as for  "Is it OK to use both ipu1 and hdmi tx audio?" - BSP does not

use SDMA for IPU operations, therefore it is possible both modules at the same

time.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复