About selects between two possible sources for SDMA_EVENT in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About selects between two possible sources for SDMA_EVENT in i.MX6DQ.

Jump to solution
1,014 Views
keitanagashima
Senior Contributor I

Dear all,

Hello. I have a question about selection between two possible sources for SDMA_EVENT in i.MX6DQ.

BSP: L3.0.35_4.1.0

Refer to "IOMUXC_GPR0 field descriptions" in MCIMX6DQRMM(Rev.2).

DMAREQ_MUX_SEL0 bit of register IOMUXC_GPR0, let us to Selects between two possible sources for SDMA_EVENT[2]:

0 ipu1.ipu_sdma_event  (we think it is related with ipu1)

1 hdmi_tx.hdmi_tx_ophydtb[0] (we think it is related with hdmi tx audio)

[Question]

Is it OK to use both ipu1 and hdmi tx audio?

If it is not OK and we want to use both ipu1 and hdmi tx audio at the same time, could you help us to provide the method?

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
951 Views
Yuri
NXP Employee
NXP Employee

Hello,

  as for  "Is it OK to use both ipu1 and hdmi tx audio?" - BSP does not

use SDMA for IPU operations, therefore it is possible both modules at the same

time.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
952 Views
Yuri
NXP Employee
NXP Employee

Hello,

  as for  "Is it OK to use both ipu1 and hdmi tx audio?" - BSP does not

use SDMA for IPU operations, therefore it is possible both modules at the same

time.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply