About secure boot KPI keys

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About secure boot KPI keys

Jump to solution
2,033 Views
changbaoma
Contributor IV

When generate KPI keys tree used in secure boot by hab4_pki_tree.sh.

What is the maximum years of the PKI tree keys duration?

What would happen if this max duration is expired?

0 Kudos
Reply
1 Solution
1,991 Views
Yuri
NXP Employee
NXP Employee

@changbaoma 
Hello,

   Customers can try to input 200 or 1000 years.
Note: i.MX devices are qualified for 10 - 15 years on continuous operation.

Regards,
Yuri.

View solution in original post

5 Replies
2,014 Views
changbaoma
Contributor IV

Hi, Yuri

I have read your post above, but also confuse me.

What is the maximum duration can i set? 10 years?  or 1000 years? or more?

If the KPI keys are valid for 10 years, can the current generated KPI keys be used to sign a new image after 10 years?  Or i must to generated new KPI keys at that time.

0 Kudos
Reply
2,008 Views
Yuri
NXP Employee
NXP Employee

Use 10 year - no need to modify the keys after this period.

 

~Yuri.

0 Kudos
Reply
2,005 Views
changbaoma
Contributor IV

Our customs may use our products 50 years,even 200 years. 

During this period, we need to do equipment maintenance all the time, and will still upgrade and re-sign zImage.

can we input 200 (years) even 1000 years? @Yuri 

0 Kudos
Reply
1,992 Views
Yuri
NXP Employee
NXP Employee

@changbaoma 
Hello,

   Customers can try to input 200 or 1000 years.
Note: i.MX devices are qualified for 10 - 15 years on continuous operation.

Regards,
Yuri.