About secure boot KPI keys

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About secure boot KPI keys

ソリューションへジャンプ
3,332件の閲覧回数
changbaoma
Contributor IV

When generate KPI keys tree used in secure boot by hab4_pki_tree.sh.

What is the maximum years of the PKI tree keys duration?

What would happen if this max duration is expired?

0 件の賞賛
返信
1 解決策
3,290件の閲覧回数
Yuri
NXP Employee
NXP Employee

@changbaoma 
Hello,

   Customers can try to input 200 or 1000 years.
Note: i.MX devices are qualified for 10 - 15 years on continuous operation.

Regards,
Yuri.

元の投稿で解決策を見る

5 返答(返信)
3,313件の閲覧回数
changbaoma
Contributor IV

Hi, Yuri

I have read your post above, but also confuse me.

What is the maximum duration can i set? 10 years?  or 1000 years? or more?

If the KPI keys are valid for 10 years, can the current generated KPI keys be used to sign a new image after 10 years?  Or i must to generated new KPI keys at that time.

0 件の賞賛
返信
3,307件の閲覧回数
Yuri
NXP Employee
NXP Employee

Use 10 year - no need to modify the keys after this period.

 

~Yuri.

0 件の賞賛
返信
3,304件の閲覧回数
changbaoma
Contributor IV

Our customs may use our products 50 years,even 200 years. 

During this period, we need to do equipment maintenance all the time, and will still upgrade and re-sign zImage.

can we input 200 (years) even 1000 years? @Yuri 

0 件の賞賛
返信
3,291件の閲覧回数
Yuri
NXP Employee
NXP Employee

@changbaoma 
Hello,

   Customers can try to input 200 or 1000 years.
Note: i.MX devices are qualified for 10 - 15 years on continuous operation.

Regards,
Yuri.