Hello community,
The IMX6DQCE errata sheet [ERR006282] points out three problems.
1) PFD is in an unknown state during boot.
2) Reprogramming PLL2/ PLL3
3) Suspend & Resume with PLL2/PLL3 bypassed.
1) is fixed by silicon revision 1.3
2) is fixed by u-boot patch.
But 3) it would be affected by software setting. so it have no patch and must care by user I think.
In default setting of Linux/Android BSP, is it cared?
Q1.
Is the standard BSP implemented so that it does not conflict with this errata?
Q2.
If so, which type of implementation of each linux/android BSP to avoid it?
1) Are BSP set respective PFDx_CLKGATE bits because PLL is bypassed.
2) BSP is not set PLL bypass mode.
Q3.
Doe's it have any possibility to set pll bypassed?
Like a
* Enable serial console as stand-up source.
* Enable a resume function as USB device.
I look forward to hearing from you.
Best regards,
Ishii.
已解决! 转到解答。
Hi Ishii
>Q1.Is the standard BSP implemented so that it does not conflict with this errata?
yes
>Q2.If so, which type of implementation of each linux/android BSP to avoid it?
BSP does not set PLL bypass mode.
>Q3. Doe's it have any possibility to set pll bypassed?
standard BSP does not use pll bypassed.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ishii
>Q1.Is the standard BSP implemented so that it does not conflict with this errata?
yes
>Q2.If so, which type of implementation of each linux/android BSP to avoid it?
BSP does not set PLL bypass mode.
>Q3. Doe's it have any possibility to set pll bypassed?
standard BSP does not use pll bypassed.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------